This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3135: CC3135&Radio tool

Part Number: CC3135

Hello Team,

When I use radioToolcli. exe with RadioTool, I use one CC3135 as TX and one CC3135 as RX.The CLI commands are tx:  \ RadioToolcli. exe -x1 -p57 -b115200  -t -z1-c4 -M1-w15 -n0 -t5 -v "and Rx:".\ RadioToolcli. exe -x1 -p38 -b115200 -c4 -r  -x 0123456789AB -q -t5 -v",  Two Radiotoolcli. exe can be used on Windows 10, but can not be used on Windows 7 as both TX and RX tools  at the same time, Once both RadioToolcli.exe are connected at the same time, one of them will pop up an error dialog indicating that radioToolcli.exe has stopped working, May I ask whether your company has made restrictions on this aspect?

Looking forward to your reply.

Zhang