Other Parts Discussed in Thread: UNIFLASH, , , CC3100
Hello,
I have again the same problem like the last time. See related question. The last time I thought that the hardware is defect, but I'm not so sure anymore.
The problem is still the same: Instead of measuring the time between flags on the pin2, it's measuring somehow the RTC frequency. On the Evalboard (CC3200-Lauchxl) was it working but on the real hardware not.
But this time I was able to reproduce this issue with the CC3200-Lauchxl board! And it doesn't matter what software I put with the debugger on the board it is now also measuring the RTC and not pin2.
Normally I was flashing the Evalboard via the internal TI debugger directly from the IAR environment. The real hardware was flashed via UART and uniflash. I tried now the same with the evalboard and here we go the problem is the same... and the really strange thing is that it doesn't matter what software I flash with the debugger the problems stays the same. But the software is still be flashed! When I change a pin from low to high it is working.
So something is the uniflash doing that has impact on the behavior on pin2 edge detection and even overwriting the software with the debugger is not changing it.
Some clues what it could be?