Hi,
I'm trying to better understand the calibrator set_tx_power command.
The first argument is the power level. My question is, do the BO and trace loss settings in the INI file take affect assuming I have channel limitation set to 1 (enabled)?
For example, lets say my INI has a trace loss defined as 3dBm and my BO ends up being 7dBm. (lets assume my Power Limits are max in the INI)
When I use the following calibrator command, what power should I expect at the output of the module, i.e. at the U.FL connector?
calibrator set_tx_power 16000 0 0 1 0 0 0 1 0 0 0 0
Would I expect to see 16dBm at the output or would I expect to see 16-7-3 = 6 dBm at the output?
Thanks