Other Parts Discussed in Thread: UNIFLASH,
Hi
I am working to create a script to automate our file system loading for the MCU image and aws certificates. I can get the script to successfully run but the program no longer reads the AWS certificates(shown below) when i program the unit from the bash console.


When i manually load the certificates through uniflash it works fine(setup shown below).


*the second iot_id.txt was when i overwrote the file but it shows up as a seperate file.
here is the script:
./detect-devices.bat
./dslite.bat --mode cc32xx project new --name My_Test_Project --device CC3235SF --mode development –overwrite
./dslite.bat --mode cc32xx project add_file --name My_Test_Project –-file C:/ti/uniflash_7.0.0/dummy-root-ca-cert --fs_path dummy-root-ca-cert
./dslite.bat --mode cc32xx project add_file --name My_Test_Project --file C:/ti/uniflash_7.0.0/tisigner.crt.der --fs_path tisigner.crt.der
./dslite.bat --mode cc32xx project add_file --name My_Test_Project --file C:/ti/uniflash_7.0.0/ce19e27d65-certificate.pem.crt --fs_path root/cert/aws-cert.pem.crt --flags vendor --token 1952007250 --cert tisigner.crt.der --priv C:/ti/uniflash_7.0.0/tisigner.key --overwrite
./dslite.bat --mode cc32xx project add_file --name My_Test_Project --file C:/ti/uniflash_7.0.0/ce19e27d65-private.pem.key --fs_path root/cert/aws-private.pem.key --flags vendor --token 1952007250 --priv C:/ti/uniflash_7.0.0/tisigner.key --cert tisigner.crt.der --overwrite
./dslite.bat --mode cc32xx project add_file --name My_Test_Project --file C:/ti/uniflash_7.0.0/thing_name.txt --fs_path root/cert/iot_id.txt --flags vendor --token 1952007250 --priv C:/ti/uniflash_7.0.0/tisigner.key --cert tisigner.crt.der --overwrite
./dslite.bat --mode cc32xx project add_file --name My_Test_Project --file C:/ti/uniflash_7.0.0/leafi_firmware_0.1.2-rc4.bin --mcu --flags vendor --token 1952007250 --priv C:/ti/uniflash_7.0.0/tisigner.key --cert tisigner.crt.der --max_size 1048576 --overwrite
./dslite.bat --mode cc32xx project set_sp --name My_Test_Project --file C:/ti/uniflash_7.0.0/4.1.0.28_3.1.0.5_3.1.0.17.bin
./dslite.bat --mode cc32xx project set_certstore --name My_Test_Project --file C:/ti/uniflash_7.0.0/certcatalogPlayGround20160911.lst --sign C:/ti/uniflash_7.0.0/certcatalogPlayGround20160911.lst.signed_3235.bin
./dslite.bat --mode cc32xx device info
./dslite.bat --mode cc32xx project program --name My_Test_Project --dev
Thanks.