This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3235MODAS: What transmission speed can I achieve with the CC3235MOD in an application as described?

Part Number: CC3235MODAS

Hi TI,

I need to develop a wifi application that takes an http data stream, encrypts it and sends it via web socket.

What transmission speed can I achieve with the CC3235MOD in an application as described above?

How many data streams can I have simulataneously?

Thank yuo very much. 

Best ragrds. 

  • Hello Albgarc2014,

    The datasheet for the CC3235MODAS specifies that the application throughput of the device depends on whether TCP or UDP is implemented: 

    Additionally, there are 16 BSD sockets available on the device to be used with internet and application protocols. 

    Best,

    -Ryan