Other Parts Discussed in Thread: UNIFLASH, CC3235MODS, LAUNCHXL-CC3235S, SYSCONFIG, CC3235S, SYSBIOS
Hi
We are currently debugging a product using CC3235MODAS.
We wrote the CC3235MODAS program from CCR and it finished normally, but it doesn't seem to be running.
As a confirmation of operation, we toggle GPIO every time we go through the main() loop, but there is no response.
As I posted last time, we can't even debug via JTAG because we can't set the TCK pin correctly, so we have no idea what's going on.
(Article: CC3235MODAS: JTAG_TCK cannnot set the module pin21)
So I have a question,
1. Is it correct to recognize that if there is no external Flash with the CC3235MODAS configuration, writing the program in CCR will be written to the built-in ROM?
2. Does CC3235MODAS absolutely require an external Flash?