Hi,
I have an issue when using sl_Send of payload of around 939 bytes, a fatal error SL_DEVICE_EVENT_FATAL_DRIVER_ABORT occurs. But when using payload of less than 500 bytes it is working fine.
I am aware that sl_Send is capable of handling up to 1460 bytes but why is it that there is an error even at 939 bytes? Is there a way to get around this and use up to 1460 bytes?
We are using UART as communication line between CC3135MOD and the MCU. Is there a limitation when using UART in terms of the bytes sent?
Thanks in advance.