Other Parts Discussed in Thread: WL1837MOD
Hi Guys,
I am currently resolving an issue where we noticed that a small batch of devices that we shipped to customers that were using the WL1835MOD module had a WL1837MOD wl18xx-conf.bin file by mistake.
We haven't had any reports of issues with those devices, but we caught the problem during a review when revising the product to use the WL1837MOD for future batches of the device.
Whilst we are working on an update to fix the issue, I wanted to know until the fix is rolled out, if there are any negative side effects we should be aware of with the WL1835MOD running the WL1837MOD wl18xx-conf.bin?
There is a small amount of differences between the two configs, which are shown below.
--- wl1835-conf.conf +++ wl1837-conf.conf -wl18xx.phy.high_band_component_type = 0x09 +wl18xx.phy.high_band_component_type = 0x0a -wl18xx.phy.number_of_assembled_ant5 = 0x00 +wl18xx.phy.number_of_assembled_ant5 = 0x02 -wl18xx.phy.per_chan_pwr_limit_arr_11abg = 0x78, 0x88, 0x88, 0x78, 0x88, 0x88, 0x78, 0x88, 0x88, 0x78, 0x88, 0x88, 0x78, 0x88, 0x18, 0x78, 0x88, 0x88, 0x78, 0x88, 0x82, 0x78, 0x88, 0x88, 0x78, 0x88, 0x88, 0x78, 0x88, 0x88, 0x78, 0x88, 0x88, 0x78, 0x88, 0x88, 0x78, 0x88, 0x88, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff +wl18xx.phy.per_chan_pwr_limit_arr_11abg = 0x78, 0x88, 0x88, 0x78, 0x88, 0x88, 0x78, 0x88, 0x88, 0x78, 0x88, 0x88, 0x78, 0x88, 0x18, 0x78, 0x88, 0x88, 0x78, 0x88, 0x82, 0x78, 0x88, 0x88, 0x78, 0x88, 0x88, 0x78, 0x88, 0x88, 0x78, 0x88, 0x88, 0x78, 0x88, 0x88, 0x78, 0x88, 0x88, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xf7, 0x22, 0x22, 0xff, 0xff, 0xff, 0xf7, 0x22, 0x22, 0xff, 0xff, 0xff, 0xf7, 0xff, 0xff, 0xff, 0xff, 0xff, 0xf7, 0xff, 0xff, 0xf4, 0x44, 0xff, 0xf4, 0x44, 0xff, 0xf4, 0x22, 0x22, 0xf4, 0x22, 0x22, 0xf6, 0x44, 0x44, 0xff, 0x44, 0x44, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0x55, 0xff, 0x44, 0x55, 0xf4, 0xff, 0xff, 0xff, 0x33, 0x22, 0xff, 0x33, 0x22, 0xff, 0x66, 0x66, 0xff, 0x44, 0x66, 0xf6, 0xff, 0xff, 0xff, 0xff, 0xff -wl18xx.phy.per_chan_bo_mode_11_abg = 0x40, 0x00, 0x04, 0x30, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x19 +wl18xx.phy.per_chan_bo_mode_11_abg = 0x40, 0x00, 0x04, 0x30, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x40, 0x19 -wl18xx.phy.per_chan_bo_mode_11_p = 0x00, 0x00, 0x00, 0x00 +wl18xx.phy.per_chan_bo_mode_11_p = 0x00, 0x00, 0x00, 0x01 -wl18xx.phy.per_sub_band_tx_trace_loss = 0x10, 0x10, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00 +wl18xx.phy.per_sub_band_tx_trace_loss = 0x08, 0x18, 0x10, 0x10, 0x10, 0x10, 0x10, 0x10, 0x10, 0x10 -wl18xx.phy.per_sub_band_rx_trace_loss = 0x10, 0x10, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00 +wl18xx.phy.per_sub_band_rx_trace_loss = 0x08, 0x18, 0x10, 0x10, 0x10, 0x10, 0x10, 0x10, 0x10, 0x10, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00