The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3235SF: CC3235MODASF12MON cannot write to the built-in flash

Part Number: CC3235SF
Other Parts Discussed in Thread: UNIFLASH, LAUNCHCC3235MOD,

I connected the XDS110 on LAUNCH CC3235MOD to CC3235MODASF12MON and tried to write a binary file with UniFlash, but the following error occurred and I could not write.

-------------------------------------------------- -------------------------------------------------- ----------
[XXXXXX] [INFO] Cortex_M4_0: Please check if the image built is based on the connected device
[XXXXXX] [INFO] Cortex_M4_0: Image Creator tool generates specific SLI image based on the device properties
[XXXXXX] [ERROR] Cortex_M4_0: Post programming was unsuccessfully executed
[XXXXXX] [ERROR] Cortex_M4_0: [ERROR_MESSAGE]Process is failed!
-------------------------------------------------- -------------------------------------------------- ----------

In the following forum, there was a note that binary files cannot be written without connecting an external flash.
However, although the LAUNCH CC3235MOD does not have an external flash, it can be written with XDS110 + UniFlash.

e2e.ti.com/.../cc3235sf-uniflash-error-when-flashing-to-a-cc3235sf- based-hardware

What's the difference?

Best Regard.