Other Parts Discussed in Thread: CC3200
Hi,
I am working on LP-CC1352P7-4 launxl, which is connected to CC3200AUDBOOST Card.
Basically i am using I2Secho example provided and it seem to work. But when i wanted to use ONboard microphone, i am unable to get any data in buffer.
Is the Macro definations listed in I2S.h , are correct and applicable for CC3200AUDBOOST ?
I am using following defination:
#define AudioCodec_MIC_ONBOARD (0x04) // Onboard mic device
and calling
/* Configure Codec */
status = AudioCodec_config(AudioCodec_TI_3254, AudioCodec_16_BIT,
SAMPLE_RATE, AudioCodec_MONO, AudioCodec_SPEAKER_HP,
AudioCodec_MIC_ONBOARD);
to configure the Audiocodec.
But i am unable to get any microphone data in buffer, whereas same buffer gets filled if i feed via Line_in via mobile.
Is there anything that i am missing ?
Can you please help.