Other Parts Discussed in Thread: UNIFLASH, CC3235S
Hi
I'm wanting to replace the default out of box application with my version of the netwrok terminal example application so that on powerup my application runs rather than the OOB application.
Currently, when i use CCS to load/debug my application, it is all fine until i repower the launchpad whereupon the outOfBox OOB app executes rather than my app.
I have tried to use to Uniflash but am unclear which specific bin/out files i need to load from the project mcu+image folder.
I have tried.....
From the initial window of uniflash I selected the "create session from Existing target configuration file" and then the ccxml file in the network terminal project folder "targetConfigs" .
I then clicked "start" (not start image creator) and entered the window where i need to select the flash images.....
i selected "network_terminal_CC3235S_LAUNCHXL_tirtos_ccs.out" from the MCU+image folder which loaded the app & all was fine UNTIL i cycled the power (or pressed reset - SW1) at which point the default OOB app ran.
The SOP jumpers are set as 010 as per SWRU539.pdf
thank in advance
thanks in advance.