Other Parts Discussed in Thread: CC3135
Hi,
I'd like to share with you my observations regarding actual DTIM value.
I have a setup of two WiFi Access Points (Linksys EA 6900 and Anatel Unifi 6 Lite) and two WiFi modules (CC3135 and similar one from another vendor). All described activities are on 5 GHz band.
CC3135 module info:
NWP 4.12.0.1
MAC 3.7.0.1
PHY 3.1.0.26
ChipId 823132160
ROM 8738
Scenario: Having DTIM value set to 300, associate the module to AP and check consumption graphs - actual DTIM value is monitored via consumption spikes.
Results:
- CC3135 and Linksys EA 6900: OK, DTIM 300
- CC3135 and Anatel Unifi 6 Lite: ERROR, DTIM 100
- another vendor and Linksys EA 6900: OK, DTIM 300
- another vendor and Anatel Unifi 6 Lite: OK, DTIM 300
So, unexpected results are observed for a combination of CC3135 and Anatel Unifi 6 Lite. Reading DTIM value setting back form the CC3135 gives 300, as configured, where actual measured value is 100.
Is this a known behavior and there are some incompatibility issues with few WiFi AP models ?
Best.