Hello,
Does the CC3100 support testing using the loopback address (127.0.0.1-127.255.255.255) on a specific port (e.g., 80)?
If so, how can I test if the HTTP server is enabled or not this way?
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Does the CC3100 support testing using the loopback address (127.0.0.1-127.255.255.255) on a specific port (e.g., 80)?
If so, how can I test if the HTTP server is enabled or not this way?
Thank you
It's possible to determine this checking the Netapp state? I've tried all the available APIs and couldn't get them tell me if the HTTP server was enabled or not. The only way I can determine if it's running is by reading the sys/mode.cfg
file.
Hi,
You have right, there is no API to get state of http server. You can "determine" state of webserver from return code of sl_NetAppStart() or error from asynchronous handler if something failed.
Jan