Hi,
I'm using SDK 6.10, and I changed the project written in sl_* to SlNet* to use the OTA_IF module. (I'm referring to the mqtt_client example)
I'm use the WIFI_IF_reset() API(it called SlWiFiConn_reset() API) of the WiFi_IF module for the operation of restarting the network processor for network or WLAN setting (eg, DHCP or WLAN operation channel).
After the image is programmed, Reset API returns almost immediately, but after a certain situation (which happened when CC3235S is turned on for a long time), there is a delay of 2-3 seconds before returning.
If there is a delay, the same occurs even after rebooting the CC3235S.
I did not find this situation when calling sl_stop() and sl_start() in the existing project.
Attached file is the NWP log when Reset returns immediately and when delay occurs.
(In each log, the Reset operation was performed a total of 3 times.)
Please let me know why the delay is occurring and how to fix it.
Thansk.