Other Parts Discussed in Thread: SYSCONFIG
Hi,
Thanks to this forum, I end up development phase of CC3235MODS project.
When we implemented these modules in the target factory and did test running, We found that
we need to improve coverage between devices. As this is an IoT application, I use 5GHz mode
in transceiver mode. The current parameters are as follows:
- Channel : 165
- RF power: 15
- Modulation: SL_WLAN_RATE_24M
- RF packet length: <60 bytes
- Antenna: dipole, 1 or 2dBi
- RF preamble: SL_WLAN_LONG_PREAMBLE
- What else?
Maximum distance between the devices are less than 30m. There is no wall between them, but various equipment made of steel.
What could you recommend to increase the communication success ratio?
Berards,
J.Y. Kim