Hello,
I'm using Free RTOS with NWP v2.14.0.0. I keep hitting an assert when I call sl_ExtLib_MqttClientCtxCreate(). Below is the sequence of SL_x calls for different scenarios that I've tried.
1. Power on CC3100
2. sl_Start
- WiFi profile already exists
3. sl_ExtLib_MqttClientInit
- interrupt comes in and IP's are received
4. Ensure client context is disconnected and deleted: sl_ExtLib_MqttClientDisconnect & sl_ExtLib_MqttClientCtxDelete
5. sl_ExtLib_MqttClientCtxCreate
- ID's, Will Params, etc are set.
6. sl_ExtLib_MqttClientConnect
7. sl_ExtLib_MqttClientSub
^ this is the normal connection flow that I use and works well.
I've been trying to implement a way to reset the mqtt session and restart the CC3100 without needing to restart the host MCU. This is what I'm doing for that:
1. sl_ExtLib_MqttClientUnsub
2. Ensure client context is disconnected and deleted: sl_ExtLib_MqttClientDisconnect & sl_ExtLib_MqttClientCtxDelete
3. sl_ExtLib_MqttClientExit
4. sl_Stop
5. Power off CC3100
6. Start the same steps as shown in the previous section but now an assert happens in sl_ExtLib_MqttClientCtxCreate -> mqtt_client_ctx_create -> MUTEX_UNLOCK() -> xQueueGenericSend
- Specifically the assert in FREE RTOS's queue.c:
...
#if ( ( INCLUDE_xTaskGetSchedulerState == 1 ) || ( configUSE_TIMERS == 1 ) )
{
configASSERT( !( ( xTaskGetSchedulerState() == taskSCHEDULER_SUSPENDED ) && ( xTicksToWait != 0 ) ) );
}
#endif
...
It seems like the scheduler is suspended when it gets here.
Any insight on why this might be happening? Or can I get some guidance on a better way to implement a "reset WiFi" api?