Hello,
Currently we are facing some problems on the Wi-Fi connection stability: it disconnects and connects several times during the day.
(this capture in on 137 end-point)
We can observe here two situations:
- It looks like that 239 end-point does not receive nothing during 5 minutes and the it triggers the keep-alive message
- 239 end-point sends a TCP Window Update but, since it does not receive nothing during 60s, it triggers the FIN
- 137 end-point is answering to the TCP Window Update but already after the FIN
- Do you see that we should decrease SL_SO_KEEPALIVETIME to 4 minutes in 239 end-point side? currently it is 5 on both
- Should we increase this 60s timeout? If so, how can we increase it?
Thank you.