This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3220SF-LAUNCHXL: AZURE based OTA support.

Part Number: CC3220SF-LAUNCHXL

HI Support, 

I have been using the Azure SDK v4_10_01_01 in a project. I want to implement OTA with the Present SDK. I recently found out that Azure provides an Device Upgrade (OTA) feature. 

Is there any TI based sample example or demo project that has Device Update feature. If yes please provide the links for the sample.

Here is the reference links:- Understand Device Update for Azure IoT Hub Agent | Microsoft Learn

azure-iot-middleware-freertos/how_to_use_adu_client.md at main · Azure/azure-iot-middleware-freertos · GitHub

Thanks,

Sai Jnaneswar Juvvisetty