Part Number: CC3135MOD
Hi
I am now looking at SWPA231 CC313x Wi-Fi Embedded Programming app note which is using UART interface to program CC3135MOD Flash from third party MCU.
and I am using SPI interface between CC3135MOD and STM MCU, and trying to program/update CC3135MOD flash from MCU via SPI.
However, I could not find any related documents to use SPI interface to program CC3135MOD flash from host MCU
So, I wonder if the embedded programming from MCU via SPI interface is the same as via UART interface?
If not so, what other steps I need to take care of when using SPI interface?
Looking forward hearing the answer very soon
Thanks