Other Parts Discussed in Thread: BEEPROG
Hi,
Just want to confirm that the 32Mbit SPI serial flash is integrated in the module?
If it is integrated can the External SPI Programming port be used for additional memory.
Thanks,
Liam
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Just want to confirm that the 32Mbit SPI serial flash is integrated in the module?
If it is integrated can the External SPI Programming port be used for additional memory.
Thanks,
Liam
Hi Jan,
The spec states 32MB SFLASH Comparison table (Table 6.2) in the spec (Link below). Just to confirm is it 4MB or 32MB of SFLASH
Thanks,
Liam
Hi Jan
Thanks for confirming.
One last question, want to get my head round the External SPI Programming interface.
I don't see an option when selecting Modules to exclude the 32MB SFLASH and add your own. So wondering what the External SPI programming interface is used for.
Is this for an external device to allow read/write access to the 32MB SFLASH contained in the Module?
Thanks,
Liam
Hi Liam,
All CC32xx modules from TI have integrated SPI flash. There is no option to obtain module without internal 32-Mbit sFlash.
Module contain SPI flash from Macronix (MX25R3235F). If you want program SPI flash other way that using UART bootlaoder from module, you can you 3rd party flash programmer (e.g. TOTAL PHASE CHEETAH, Elnec Beeprog 2,...).
Jan