This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3235S: connecting to the CC3235S custom board issue

Part Number: CC3235S
Other Parts Discussed in Thread: UNIFLASH

Hi All,

I have designed a custom board based on CC3235S (replicate the design, provided in the datasheet). It powers up properly, and I can see the 1.9 and 1.2 volts on the DCDC ANA and DIG outputs.

The SOP pins are configured as 010 as suggested by the documentations.

Trying to connect to the device in uni flash via serial port, it just keep returning 'timeout' error.  I have also tried different SOP configurations as well. 

Re the programmer, I am using a Launch-CC3235S board to program the MCU; RX, TX and RST pins from the Launch-CC3235S headers are connected to the custom board. The connections have been carefully checked.

Is there any hint on what could be the potential issue, or any suggestion for fault finding?

Any help is really appreciated.