This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3300: cc33xx-nvs issue

Part Number: CC3300
Other Parts Discussed in Thread: SK-AM62B-P1, CC3301

Tool/software:

Dear expert,

I encountered a similar issue here :

SDK version: ti-processor-sdk-linux-am335x-evm-09.01.00.001/cc33xx/cc33xx_rootfs . Pls check the let me know if there an update for fix the issue . Thanks.

root@am62xx-evm:~# dmesg | grep 33
[    0.033556] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[    0.333772] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[    0.369331] platform connector: Fixed dependency cycle(s) with /bus@f0000/i2c@20010000/sii9022@3b
[    0.480633] usbcore: registered new interface driver hub
[    0.596833] TCP bind hash table entries: 16384 (order: 7, 524288 bytes, linear)
[    0.783347] io scheduler kyber registered
[    0.933166] sdhci: Secure Digital Host Controller Interface driver
[    0.989633] optee: initialized driver
[    1.278338] omap8250 2810000.serial: PM domain pd:152 will not be powered off
[    3.873375] systemd[1]: Starting Load Kernel Module fuse...
[    3.922330] systemd[1]: Starting Start psplash boot splash screen...
[    4.871266] audit: type=1334 audit(1651167747.940:2): prog-id=5 op=LOAD
[    4.878115] audit: type=1334 audit(1651167747.948:3): prog-id=6 op=LOAD
[    5.980833] rtc-ti-k3 2b1f0000.rtc: registered as rtc0
[    6.337507] platform 78000000.r5f: R5F core may have been powered on by a different host, programmed state (0) != actual state (1)
[    6.348046] cc33xx_sdio mmc2:0001:2: Using GPIO as IRQ
[    6.840909] audit: type=1334 audit(13.348:4): prog-id=7 op=LOAD
[    6.853662] audit: type=1334 audit(13.364:5): prog-id=8 op=LOAD
[    9.024129] wlcore: cc33xx_probe :: Start
[    9.024822] wlcore: WLAN CC33xx platform device probe done
[    9.029207] cc33xx_driver cc33xx.3.auto: Direct firmware load for ti-connectivity/cc33xx-nvs.bin failed with error -2
[    9.040777] wlcore: Could not get nvs file ti-connectivity/cc33xx-nvs.bin
[    9.291759] audit: type=1334 audit(15.800:6): prog-id=9 op=LOAD
[    9.298873] audit: type=1334 audit(15.808:7): prog-id=10 op=LOAD
[    9.333010] wlcore: Set BLKsize to 128
[    9.333052] IBI_WA: Read core status
[    9.333138] wlcore: BOOT IRQs: 0x8
[    9.333153] IBI_WA: Core status processed

Regards,

Fredy Zhang

  • I am using those two boards:

    SK-AM62B-P1 and M2-CC3301

  • The cc33xx-nvs.bin failed with error -2 is due to the NVS file not being present, however the default MAC address from TI will be used otherwise. If you would like to override the default MAC Address, you can do so by creating a file in the Linux filesystem in the  the /lib/firmware/ti-connectivity directory and named cc33xx-nvs.bin 

    Creation of the cc33xx-nvs.bin file is done with the following command with the example MAC “AA:BB:CC:DD:EE:FF”:

    echo -n -e '\xAA\xBB\xCC\xDD\xEE\xFF' > /lib/firmware/ti-connectivity/cc33xx-nvs.bin

    BR,

    Christina

  • Dear,

    Christina, I still can't find the WLAN node on the device . Pls help to check . Thanks.

    [    6.489363] cc33xx_sdio mmc2:0001:2: Using GPIO as IRQ
             Starting DEMO...
             Starting Print notice about GPLv3 packages...
             Starting IPv6 Packet Filtering Framework...
             Starting IPv4 Packet Filtering Framework...
    [  OK  ] Started irqbalance daemon.
             Starting Telephony service...
             Starting PulseAudio Sound System...
             Starting Expand the rootfs…ll size of the boot device....
    [  OK  ] Started strongSwan IPsec I…IKEv2 daemon using ipsec.conf.
    [    6.730694] audit: type=1334 audit(12.348:4): prog-id=7 op=LOAD
    [    6.742790] audit: type=1334 audit(12.360:5): prog-id=8 op=LOAD
             Starting User Login Management...
    [  OK  ] Started TEE Supplicant.
             Starting Telnet Server...
    [  OK  ] Started ti-apps-launcher service.
    

    root@am62xx-evm:~# ifconfig
    eth0: flags=4099<UP,BROADCAST,MULTICAST>  mtu 1500
            ether 1c:63:49:22:50:18  txqueuelen 1000  (Ethernet)
            RX packets 0  bytes 0 (0.0 B)
            RX errors 0  dropped 0  overruns 0  frame 0
            TX packets 0  bytes 0 (0.0 B)
            TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0
    
    eth1: flags=4099<UP,BROADCAST,MULTICAST>  mtu 1500
            ether 70:ff:76:1e:d1:ac  txqueuelen 1000  (Ethernet)
            RX packets 0  bytes 0 (0.0 B)
            RX errors 0  dropped 0  overruns 0  frame 0
            TX packets 0  bytes 0 (0.0 B)
            TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0
    
    lo: flags=73<UP,LOOPBACK,RUNNING>  mtu 65536
            inet 127.0.0.1  netmask 255.0.0.0
            inet6 ::1  prefixlen 128  scopeid 0x10<host>
            loop  txqueuelen 1000  (Local Loopback)
            RX packets 93  bytes 7714 (7.5 KiB)
            RX errors 0  dropped 0  overruns 0  frame 0
            TX packets 93  bytes 7714 (7.5 KiB)
            TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0
    

  • Hi,

    Could we get the full log? This doesn't show everything.

    Thanks,

    Christina

  • Christina

    Pls help to check . Thanks. 

    3630.minicom.txt
    fan
    Password: 
    U-Boot SPL 2023.04-gb0d717b732 (Dec 06 2023 - 15:11:45 +0000)
    SYSFW ABI: 3.1 (firmware rev 0x0009 '9.1.8--v09.01.08 (Kool Koala)')
    SPL initial stack usage: 13384 bytes
    Trying to boot from MMC2
    Authentication passed
    Authentication passed
    Authentication passed
    Authentication passed
    Authentication passed
    Starting ATF on ARM64 core...
    
    NOTICE:  BL31: v2.9(release):v2.9.0-614-gd7a7135d32-dirty
    NOTICE:  BL31: Built : 09:34:15, Aug 24 2023
    
    U-Boot SPL 2023.04-gb0d717b732 (Dec 06 2023 - 15:11:45 +0000)
    SYSFW ABI: 3.1 (firmware rev 0x0009 '9.1.8--v09.01.08 (Kool Koala)')
    SPL initial stack usage: 1856 bytes
    Trying to boot from MMC2
    Authentication passed
    Authentication passed
    
    
    U-Boot 2023.04-gb0d717b732 (Dec 06 2023 - 15:11:45 +0000)
    
    SoC:   AM62X SR1.0 HS-FS
    Model: Texas Instruments AM625 SK
    EEPROM not available at 80, trying to read at 81
    Board: AM62B-SKEVM-P1 rev A
    DRAM:  2 GiB
    Core:  72 devices, 32 uclasses, devicetree: separate
    MMC:   mmc@fa10000: 0, mmc@fa00000: 1
    Loading Environment from nowhere... OK
    In:    serial
    Out:   serial
    Err:   serial
    Net:   eth0: ethernet@8000000port@1
    Hit any key to stop autoboot:  2  1  0 
    switch to partitions #0, OK
    mmc1 is current device
    SD/MMC found on device 1
    Failed to load 'boot.scr'
    574 bytes read in 16 ms (34.2 KiB/s)
    Loaded env from uEnv.txt
    Importing environment from mmc1 ...
    ## Error: "main_cpsw0_qsgmii_phyinit" not defined
    20302336 bytes read in 230 ms (84.2 MiB/s)
    60028 bytes read in 20 ms (2.9 MiB/s)
    Working FDT set to 88000000
    ## Flattened Device Tree blob at 88000000
       Booting using the fdt blob at 0x88000000
    Working FDT set to 88000000
    ERROR: reserving fdt memory region failed (addr=ff700000 size=8ca000 flags=4)
       Loading Device Tree to 000000008feee000, end 000000008fffffff ... OK
    Working FDT set to 8feee000
    
    Starting kernel ...
    
    [    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
    [    0.000000] Linux version 6.1.46-00001-g1e52556d77ab-dirty (fredy@ubuntu22-mini) (aarch64-oe-linux-gcc (GCC) 11.4.0, GNU ld (GNU Binutils) 2.38.20220708) #1 SMP PREEMPT Sat Jun 15 23:34:03 CST 2024
    [    0.000000] Machine model: Texas Instruments AM625 SK
    [    0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '')
    [    0.000000] printk: bootconsole [ns16550a0] enabled
    [    0.000000] efi: UEFI not found.
    [    0.000000] Reserved memory: created CMA memory pool at 0x00000000f7600000, size 128 MiB
    [    0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x000000009c800000, size 3 MiB
    [    0.000000] OF: reserved mem: initialized node ipc-memories@9c800000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x000000009cb00000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node m4f-dma-memory@9cb00000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x000000009cc00000, size 14 MiB
    [    0.000000] OF: reserved mem: initialized node m4f-memory@9cc00000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x000000009da00000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node r5f-dma-memory@9da00000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x000000009db00000, size 12 MiB
    [    0.000000] OF: reserved mem: initialized node r5f-memory@9db00000, compatible id shared-dma-pool
    [    0.000000] Zone ranges:
    [    0.000000]   DMA      [mem 0x0000000080000000-0x00000000ffffffff]
    [    0.000000]   DMA32    empty
    [    0.000000]   Normal   empty
    [    0.000000] Movable zone start for each node
    [    0.000000] Early memory node ranges
    [    0.000000]   node   0: [mem 0x0000000080000000-0x000000009c7fffff]
    [    0.000000]   node   0: [mem 0x000000009c800000-0x000000009e6fffff]
    [    0.000000]   node   0: [mem 0x000000009e700000-0x000000009e77ffff]
    [    0.000000]   node   0: [mem 0x000000009e780000-0x000000009fffffff]
    [    0.000000]   node   0: [mem 0x00000000a0000000-0x00000000ff6fffff]
    [    0.000000]   node   0: [mem 0x00000000ff700000-0x00000000fffc9fff]
    [    0.000000]   node   0: [mem 0x00000000fffca000-0x00000000ffffffff]
    [    0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000ffffffff]
    [    0.000000] psci: probing for conduit method from DT.
    [    0.000000] psci: PSCIv1.1 detected in firmware.
    [    0.000000] psci: Using standard PSCI v0.2 function IDs
    [    0.000000] psci: Trusted OS migration not required
    [    0.000000] psci: SMC Calling Convention v1.4
    [    0.000000] percpu: Embedded 19 pages/cpu s37992 r8192 d31640 u77824
    [    0.000000] Detected VIPT I-cache on CPU0
    [    0.000000] CPU features: detected: GIC system register CPU interface
    [    0.000000] CPU features: detected: ARM erratum 845719
    [    0.000000] alternatives: applying boot alternatives
    [    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 516096
    [    0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 mtdparts=spi-nand0:512k(ospi.tiboot3),2m(ospi.tispl),4m(ospi.u-boot),256k(ospi.env),256k(ospi.env.backup),98048k@32m(ospi.rootfs),256k@130816k(ospi.phypattern);omap2-nand.0:2m(NAND.tiboot3),2m(NAND.tispl),2m(NAND.tiboot3.backup),4m(NAND.u-boot),256k(NAND.u-boot-env),256k(NAND.u-boot-env.backup),-(NAND.file-system) root=PARTUUID=d421661d-02 rw rootfstype=ext4 rootwait
    [    0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
    [    0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
    [    0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
    [    0.000000] Memory: 1838472K/2097152K available (12288K kernel code, 1266K rwdata, 4020K rodata, 2112K init, 438K bss, 127608K reserved, 131072K cma-reserved)
    [    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
    [    0.000000] rcu: Preemptible hierarchical RCU implementation.
    [    0.000000] rcu: 	RCU event tracing is enabled.
    [    0.000000] rcu: 	RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=4.
    [    0.000000] 	Trampoline variant of Tasks RCU enabled.
    [    0.000000] 	Tracing variant of Tasks RCU enabled.
    [    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
    [    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
    [    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
    [    0.000000] GICv3: GIC: Using split EOI/Deactivate mode
    [    0.000000] GICv3: 256 SPIs implemented
    [    0.000000] GICv3: 0 Extended SPIs implemented
    [    0.000000] Root IRQ handler: gic_handle_irq
    [    0.000000] GICv3: GICv3 features: 16 PPIs
    [    0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001880000
    [    0.000000] ITS [mem 0x01820000-0x0182ffff]
    [    0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
    [    0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19
    [    0.000000] ITS@0x0000000001820000: allocated 524288 Devices @80800000 (flat, esz 8, psz 64K, shr 0)
    [    0.000000] ITS: using cache flushing for cmd queue
    [    0.000000] GICv3: using LPI property table @0x0000000080040000
    [    0.000000] GIC: using cache flushing for LPI property table
    [    0.000000] GICv3: CPU0: using allocated LPI pending table @0x0000000080050000
    [    0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.
    [    0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys).
    [    0.000000] clocksource: arch_sys_counter: mask: 0x3ffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns
    [    0.000001] sched_clock: 58 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns
    [    0.008597] Console: colour dummy device 80x25
    [    0.013210] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000)
    [    0.023899] pid_max: default: 32768 minimum: 301
    [    0.028680] LSM: Security Framework initializing
    [    0.033559] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
    [    0.041157] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
    [    0.051330] cblist_init_generic: Setting adjustable number of callback queues.
    [    0.058809] cblist_init_generic: Setting shift to 2 and lim to 1.
    [    0.065119] cblist_init_generic: Setting adjustable number of callback queues.
    [    0.072515] cblist_init_generic: Setting shift to 2 and lim to 1.
    [    0.078924] rcu: Hierarchical SRCU implementation.
    [    0.083834] rcu: 	Max phase no-delay instances is 1000.
    [    0.089488] Platform MSI: msi-controller@1820000 domain created
    [    0.095875] PCI/MSI: /bus@f0000/interrupt-controller@1800000/msi-controller@1820000 domain created
    [    0.105313] EFI services will not be available.
    [    0.110300] smp: Bringing up secondary CPUs ...
    [    0.115690] Detected VIPT I-cache on CPU1
    [    0.115827] GICv3: CPU1: found redistributor 1 region 0:0x00000000018a0000
    [    0.115851] GICv3: CPU1: using allocated LPI pending table @0x0000000080060000
    [    0.115921] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
    [    0.116747] Detected VIPT I-cache on CPU2
    [    0.116832] GICv3: CPU2: found redistributor 2 region 0:0x00000000018c0000
    [    0.116851] GICv3: CPU2: using allocated LPI pending table @0x0000000080070000
    [    0.116883] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
    [    0.117595] Detected VIPT I-cache on CPU3
    [    0.117684] GICv3: CPU3: found redistributor 3 region 0:0x00000000018e0000
    [    0.117701] GICv3: CPU3: using allocated LPI pending table @0x0000000080080000
    [    0.117732] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
    [    0.117810] smp: Brought up 1 node, 4 CPUs
    [    0.197553] SMP: Total of 4 processors activated.
    [    0.202371] CPU features: detected: 32-bit EL0 Support
    [    0.207650] CPU features: detected: CRC32 instructions
    [    0.212982] CPU: All CPU(s) started at EL2
    [    0.217180] alternatives: applying system-wide alternatives
    [    0.225045] devtmpfs: initialized
    [    0.238289] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
    [    0.248325] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
    [    0.260829] pinctrl core: initialized pinctrl subsystem
    [    0.266968] DMI not present or invalid.
    [    0.271653] NET: Registered PF_NETLINK/PF_ROUTE protocol family
    [    0.279107] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations
    [    0.286727] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
    [    0.294859] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
    [    0.303063] audit: initializing netlink subsys (disabled)
    [    0.308805] audit: type=2000 audit(0.196:1): state=initialized audit_enabled=0 res=1
    [    0.309364] thermal_sys: Registered thermal governor 'step_wise'
    [    0.316746] thermal_sys: Registered thermal governor 'power_allocator'
    [    0.322947] cpuidle: using governor menu
    [    0.333845] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
    [    0.340884] ASID allocator initialised with 65536 entries
    [    0.357965] platform 30200000.dss: Fixed dependency cycle(s) with /bus@f0000/i2c@20010000/sii9022@3b
    [    0.369420] platform connector: Fixed dependency cycle(s) with /bus@f0000/i2c@20010000/sii9022@3b
    [    0.380889] KASLR disabled due to lack of seed
    [    0.392981] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages
    [    0.399958] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page
    [    0.406367] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages
    [    0.413308] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page
    [    0.419716] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages
    [    0.426655] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page
    [    0.433063] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages
    [    0.440002] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page
    [    0.448133] k3-chipinfo 43000014.chipid: Family:AM62X rev:SR1.0 JTAGID[0x0bb7e02f] Detected
    [    0.458981] iommu: Default domain type: Translated 
    [    0.464068] iommu: DMA domain TLB invalidation policy: strict mode 
    [    0.470835] SCSI subsystem initialized
    [    0.475110] usbcore: registered new interface driver usbfs
    [    0.480773] usbcore: registered new interface driver hub
    [    0.486265] usbcore: registered new device driver usb
    [    0.492029] pps_core: LinuxPPS API ver. 1 registered
    [    0.497108] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
    [    0.506463] PTP clock support registered
    [    0.510613] EDAC MC: Ver: 3.0.0
    [    0.514921] omap-mailbox 29000000.mailbox: omap mailbox rev 0x66fc9100
    [    0.522028] FPGA manager framework
    [    0.525600] Advanced Linux Sound Architecture Driver Initialized.
    [    0.532973] clocksource: Switched to clocksource arch_sys_counter
    [    0.539519] VFS: Disk quotas dquot_6.6.0
    [    0.543575] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
    [    0.557253] NET: Registered PF_INET protocol family
    [    0.562602] IP idents hash table entries: 32768 (order: 6, 262144 bytes, linear)
    [    0.571980] tcp_listen_portaddr_hash hash table entries: 1024 (order: 2, 16384 bytes, linear)
    [    0.580811] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
    [    0.588757] TCP established hash table entries: 16384 (order: 5, 131072 bytes, linear)
    [    0.596985] TCP bind hash table entries: 16384 (order: 7, 524288 bytes, linear)
    [    0.605124] TCP: Hash tables configured (established 16384 bind 16384)
    [    0.612067] UDP hash table entries: 1024 (order: 3, 32768 bytes, linear)
    [    0.619004] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear)
    [    0.626571] NET: Registered PF_UNIX/PF_LOCAL protocol family
    [    0.632986] RPC: Registered named UNIX socket transport module.
    [    0.639058] RPC: Registered udp transport module.
    [    0.643867] RPC: Registered tcp transport module.
    [    0.648675] RPC: Registered tcp NFSv4.1 backchannel transport module.
    [    0.655268] NET: Registered PF_XDP protocol family
    [    0.660182] PCI: CLS 0 bytes, default 64
    [    0.665196] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available
    [    0.675651] Initialise system trusted keyrings
    [    0.680546] workingset: timestamp_bits=46 max_order=19 bucket_order=0
    [    0.692134] squashfs: version 4.0 (2009/01/31) Phillip Lougher
    [    0.698872] NFS: Registering the id_resolver key type
    [    0.704100] Key type id_resolver registered
    [    0.708377] Key type id_legacy registered
    [    0.712542] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
    [    0.719396] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
    [    0.762053] Key type asymmetric registered
    [    0.766248] Asymmetric key parser 'x509' registered
    [    0.771300] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245)
    [    0.779075] io scheduler mq-deadline registered
    [    0.783714] io scheduler kyber registered
    [    0.791524] pinctrl-single 4084000.pinctrl: 34 pins, size 136
    [    0.798157] pinctrl-single f4000.pinctrl: 171 pins, size 684
    [    0.805158] pinctrl-single a40000.pinctrl: 512 pins, size 2048
    [    0.818367] Serial: 8250/16550 driver, 12 ports, IRQ sharing enabled
    [    0.836109] loop: module loaded
    [    0.840760] megasas: 07.719.03.00-rc1
    [    0.848118] tun: Universal TUN/TAP device driver, 1.6
    [    0.854194] thunder_xcv, ver 1.0
    [    0.857556] thunder_bgx, ver 1.0
    [    0.860884] nicpf, ver 1.0
    [    0.863816] e1000: Intel(R) PRO/1000 Network Driver
    [    0.868803] e1000: Copyright (c) 1999-2006 Intel Corporation.
    [    0.874721] e1000e: Intel(R) PRO/1000 Network Driver
    [    0.879796] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
    [    0.885903] igb: Intel(R) Gigabit Ethernet Network Driver
    [    0.891423] igb: Copyright (c) 2007-2014 Intel Corporation.
    [    0.897145] igbvf: Intel(R) Gigabit Virtual Function Network Driver
    [    0.903552] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
    [    0.909739] sky2: driver version 1.30
    [    0.914290] VFIO - User Level meta-driver version: 0.3
    [    0.920488] usbcore: registered new interface driver usb-storage
    [    0.927280] i2c_dev: i2c /dev entries driver
    [    0.933578] sdhci: Secure Digital Host Controller Interface driver
    [    0.939938] sdhci: Copyright(c) Pierre Ossman
    [    0.944625] sdhci-pltfm: SDHCI platform and OF driver helper
    [    0.951389] ledtrig-cpu: registered to indicate activity on CPUs
    [    0.957777] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
    [    0.964789] usbcore: registered new interface driver usbhid
    [    0.970496] usbhid: USB HID core driver
    [    0.975485] optee: probing for conduit method.
    [    0.980094] optee: revision 4.0 (2a5b1d12)
    [    0.980472] optee: dynamic shared memory is enabled
    [    0.990128] optee: initialized driver
    [    0.995949] Initializing XFRM netlink socket
    [    1.000404] NET: Registered PF_PACKET protocol family
    [    1.005667] Key type dns_resolver registered
    [    1.010576] registered taskstats version 1
    [    1.014804] Loading compiled-in X.509 certificates
    [    1.031150] ti-sci 44043000.system-controller: ABI: 3.1 (firmware rev 0x0009 '9.1.8--v09.01.08 (Kool Koala)')
    [    1.098464] omap_i2c 20000000.i2c: bus 0 rev0.12 at 400 kHz
    [    1.106358] omap_i2c 20010000.i2c: bus 1 rev0.12 at 100 kHz
    [    1.113673] omap_i2c 20020000.i2c: bus 2 rev0.12 at 400 kHz
    [    1.119712] ti-sci-intr bus@f0000:interrupt-controller@a00000: Interrupt Router 3 domain created
    [    1.129006] ti-sci-inta 48000000.interrupt-controller: Interrupt Aggregator domain 28 created
    [    1.140668] simple-framebuffer ff700000.framebuffer: framebuffer at 0xff700000, 0x8ca000 bytes
    [    1.149543] simple-framebuffer ff700000.framebuffer: format=x8r8g8b8, mode=1920x1200x32, linelength=7680
    [    1.175048] Console: switching to colour frame buffer device 240x75
    [    1.195969] simple-framebuffer ff700000.framebuffer: fb0: simplefb registered!
    [    1.204910] ti-udma 485c0100.dma-controller: Number of rings: 82
    [    1.213392] ti-udma 485c0100.dma-controller: Channels: 48 (bchan: 18, tchan: 12, rchan: 18)
    [    1.224894] ti-udma 485c0000.dma-controller: Number of rings: 150
    [    1.235566] ti-udma 485c0000.dma-controller: Channels: 35 (tchan: 20, rchan: 15)
    [    1.246081] printk: console [ttyS2] disabled
    [    1.250565] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 240, base_baud = 3000000) is a 8250
    [    1.259484] printk: console [ttyS2] enabled
    [    1.259484] printk: console [ttyS2] enabled
    [    1.267945] printk: bootconsole [ns16550a0] disabled
    [    1.267945] printk: bootconsole [ns16550a0] disabled
    [    1.278934] omap8250 2810000.serial: PM domain pd:152 will not be powered off
    [    1.286434] 2810000.serial: ttyS3 at MMIO 0x2810000 (irq = 242, base_baud = 3000000) is a 8250
    [    1.295179] serial serial0: tty port ttyS3 registered
    [    1.301724] davinci_mdio 8000f00.mdio: Configuring MDIO in manual mode
    [    1.344976] davinci_mdio 8000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
    [    1.355052] davinci_mdio 8000f00.mdio: phy[0]: device 8000f00.mdio:00, driver TI DP83867
    [    1.363185] davinci_mdio 8000f00.mdio: phy[1]: device 8000f00.mdio:01, driver TI DP83867
    [    1.363239] am65-cpsw-nuss 8000000.ethernet: initializing am65 cpsw nuss version 0x6BA01103, cpsw version 0x6BA81103 Ports: 3 quirks:00000006
    [    1.384157] am65-cpsw-nuss 8000000.ethernet: initialized cpsw ale version 1.5
    [    1.391288] am65-cpsw-nuss 8000000.ethernet: ALE Table size 512
    [    1.397853] pps pps0: new PPS source ptp0
    [    1.402242] am65-cpsw-nuss 8000000.ethernet: CPTS ver 0x4e8a010c, freq:500000000, add_val:1 pps:1
    [    1.412931] am65-cpsw-nuss 8000000.ethernet: set new flow-id-base 19
    [    1.425102] mmc0: CQHCI version 5.10
    [    1.430915] pca953x 1-0022: supply vcc not found, using dummy regulator
    [    1.437736] pca953x 1-0022: using AI
    [    1.470364] mmc0: SDHCI controller on fa10000.mmc [fa10000.mmc] using ADMA 64-bit
    [    1.471442] spi-nor spi0.0: s28hs512t (65536 Kbytes)
    [    1.482981] 7 fixed-partitions partitions found on MTD device fc40000.spi.0
    [    1.489948] Creating 7 MTD partitions on "fc40000.spi.0":
    [    1.495345] 0x000000000000-0x000000080000 : "ospi.tiboot3"
    [    1.502363] 0x000000080000-0x000000280000 : "ospi.tispl"
    [    1.508903] 0x000000280000-0x000000680000 : "ospi.u-boot"
    [    1.515503] 0x000000680000-0x0000006c0000 : "ospi.env"
    [    1.521851] 0x0000006c0000-0x000000700000 : "ospi.env.backup"
    [    1.528711] 0x000000800000-0x000003fc0000 : "ospi.rootfs"
    [    1.535392] 0x000003fc0000-0x000004000000 : "ospi.phypattern"
    [    1.551801] omap8250 2810000.serial: Failed to create device link (0x180) with regulator-7
    [    1.560332] mmc0: Command Queue Engine enabled
    [    1.562673] debugfs: Directory 'pd:182' with parent 'pm_genpd' already present!
    [    1.564846] mmc0: new HS200 MMC card at address 0001
    [    1.572440] mmc2: CQHCI version 5.10
    [    1.572534] mmc1: CQHCI version 5.10
    [    1.574714] debugfs: Directory 'pd:186' with parent 'pm_genpd' already present!
    [    1.578070] mmcblk0: mmc0:0001 S0J56X 14.8 GiB 
    [    1.586961] ALSA device list:
    [    1.593672]  mmcblk0: p1 p2
    [    1.596144]   No soundcards found.
    [    1.599916] mmcblk0boot0: mmc0:0001 S0J56X 31.5 MiB 
    [    1.611672] mmc1: SDHCI controller on fa00000.mmc [fa00000.mmc] using ADMA 64-bit
    [    1.611776] mmcblk0boot1: mmc0:0001 S0J56X 31.5 MiB 
    [    1.620999] mmc2: SDHCI controller on fa20000.mmc [fa20000.mmc] using ADMA 64-bit
    [    1.625380] mmcblk0rpmb: mmc0:0001 S0J56X 4.00 MiB, chardev (240:0)
    [    1.636744] sdhci-am654 fa20000.mmc: card claims to support voltages below defined range
    [    1.638058] Waiting for root device PARTUUID=d421661d-02...
    [    1.658298] mmc2: new high speed SDIO card at address 0001
    [    1.691694] mmc1: new ultra high speed SDR104 SDHC card at address aaaa
    [    1.699225] mmcblk1: mmc1:aaaa SC16G 14.8 GiB 
    [    1.709499]  mmcblk1: p1 p2
    [    1.997757] EXT4-fs (mmcblk1p2): recovery complete
    [    2.005489] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Quota mode: none.
    [    2.014131] VFS: Mounted root (ext4 filesystem) on device 179:98.
    [    2.024080] devtmpfs: mounted
    [    2.028843] Freeing unused kernel memory: 2112K
    [    2.033790] Run /sbin/init as init process
    [    2.200666] systemd[1]: System time before build time, advancing clock.
    [    2.266655] NET: Registered PF_INET6 protocol family
    [    2.273920] Segment Routing with IPv6
    [    2.277690] In-situ OAM (IOAM) with IPv6
    [    2.312821] systemd[1]: systemd 250.5+ running in system mode (+PAM -AUDIT -SELINUX -APPARMOR +IMA -SMACK +SECCOMP -GCRYPT -GNUTLS -OPENSSL +ACL +BLKID -CURL -ELFUTILS -FIDO2 -IDN2 -IDN -IPTC +KMOD -LIBCRYPTSETUP +LIBFDISK -PCRE2 -PWQUALITY -P11KIT -QRENCODE -BZIP2 -LZ4 -XZ -ZLIB +ZSTD -BPF_FRAMEWORK +XKBCOMMON +UTMP +SYSVINIT default-hierarchy=hybrid)
    [    2.345543] systemd[1]: Detected architecture arm64.
    
    Welcome to Arago 2023.10!
    
    [    2.449778] systemd[1]: Hostname set to <am62xx-evm>.
    [    2.602156] systemd-sysv-generator[161]: SysV service '/etc/init.d/netopeer2-server' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
    [    2.630332] systemd-sysv-generator[161]: SysV service '/etc/init.d/sysrepo' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
    [    2.655056] systemd-sysv-generator[161]: SysV service '/etc/init.d/thermal-zone-init' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
    [    2.942177] systemd[1]: Configuration file /lib/systemd/system/ti-apps-launcher.service is marked executable. Please remove executable permission bits. Proceeding anyway.
    [    3.050068] systemd[1]: /lib/systemd/system/bt-enable.service:9: Standard output type syslog is obsolete, automatically updating to journal. Please update your unit file, and consider removing the setting altogether.
    [    3.123015] systemd[1]: /etc/systemd/system/sync-clocks.service:11: Standard output type syslog is obsolete, automatically updating to journal. Please update your unit file, and consider removing the setting altogether.
    [    3.205135] systemd[1]: Queued start job for default target Graphical Interface.
    [    3.276031] systemd[1]: Created slice Slice /system/getty.
    [  OK  ] Created slice Slice /system/getty.
    [    3.300723] systemd[1]: Created slice Slice /system/modprobe.
    [  OK  ] Created slice Slice /system/modprobe.
    [    3.325499] systemd[1]: Created slice Slice /system/serial-getty.
    [  OK  ] Created slice Slice /system/serial-getty.
    [    3.351880] systemd[1]: Created slice User and Session Slice.
    [  OK  ] Created slice User and Session Slice.
    [    3.373750] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
    [  OK  ] Started Dispatch Password �ts to Console Directory Watch.
    [    3.397576] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
    [  OK  ] Started Forward Password R�uests to Wall Directory Watch.
    [    3.421820] systemd[1]: Reached target Path Units.
    [  OK  ] Reached target Path Units.
    [    3.437345] systemd[1]: Reached target Remote File Systems.
    [  OK  ] Reached target Remote File Systems.
    [    3.457373] systemd[1]: Reached target Slice Units.
    [  OK  ] Reached target Slice Units.
    [    3.473526] systemd[1]: Reached target Swaps.
    [  OK  ] Reached target Swaps.
    [    3.559427] systemd[1]: Listening on RPCbind Server Activation Socket.
    [  OK  ] Listening on RPCbind Server Activation Socket.
    [    3.581626] systemd[1]: Reached target RPC Port Mapper.
    [  OK  ] Reached target RPC Port Mapper.
    [    3.626003] systemd[1]: Listening on Process Core Dump Socket.
    [  OK  ] Listening on Process Core Dump Socket.
    [    3.650229] systemd[1]: Listening on initctl Compatibility Named Pipe.
    [  OK  ] Listening on initctl Compatibility Named Pipe.
    [    3.677274] systemd[1]: Listening on Journal Audit Socket.
    [  OK  ] Listening on Journal Audit Socket.
    [    3.704421] systemd[1]: Listening on Journal Socket (/dev/log).
    [  OK  ] Listening on Journal Socket (/dev/log).
    [    3.727014] systemd[1]: Listening on Journal Socket.
    [  OK  ] Listening on Journal Socket.
    [    3.753505] systemd[1]: Listening on Network Service Netlink Socket.
    [  OK  ] Listening on Network Service Netlink Socket.
    [    3.780817] systemd[1]: Listening on udev Control Socket.
    [  OK  ] Listening on udev Control Socket.
    [    3.803689] systemd[1]: Listening on udev Kernel Socket.
    [  OK  ] Listening on udev Kernel Socket.
    [    3.827977] systemd[1]: Listening on User Database Manager Socket.
    [  OK  ] Listening on User Database Manager Socket.
    [    3.897943] systemd[1]: Mounting Huge Pages File System...
             Mounting Huge Pages File System...
    [    3.934074] systemd[1]: Mounting POSIX Message Queue File System...
             Mounting POSIX Message Queue File System...
    [    3.993878] systemd[1]: Mounting Kernel Debug File System...
             Mounting Kernel Debug File System...
    [    4.018611] systemd[1]: Kernel Trace File System was skipped because of a failed condition check (ConditionPathExists=/sys/kernel/tracing).
    [    4.048632] systemd[1]: Mounting Temporary Directory /tmp...
             Mounting Temporary Directory /tmp...
    [    4.102344] systemd[1]: Starting Create List of Static Device Nodes...
             Starting Create List of Static Device Nodes...
    [    4.134189] systemd[1]: Starting Load Kernel Module configfs...
             Starting Load Kernel Module configfs...
    [    4.186333] systemd[1]: Starting Load Kernel Module drm...
             Starting Load Kernel Module drm...
    [    4.218693] systemd[1]: Starting Load Kernel Module fuse...
             Starting Load Kernel Module fuse...
    [    4.238408] fuse: init (API version 7.37)
    [    4.294645] systemd[1]: Starting Start psplash boot splash screen...
             Starting Start psplash boot splash screen...
    [    4.333801] systemd[1]: Starting RPC Bind...
             Starting RPC Bind...
    [    4.361803] systemd[1]: File System Check on Root Device was skipped because of a failed condition check (ConditionPathIsReadWrite=!/).
    [    4.406309] systemd[1]: Starting Journal Service...
             Starting Journal Service...
    [    4.438653] systemd[1]: Starting Load Kernel Modules...
             Starting Load Kernel Modules...
    [    4.469816] systemd[1]: Starting Generate network units from Kernel command line...
             Starting Generate network �ts from Kernel command line...
    [    4.501217] systemd[1]: Starting Remount Root and Kernel File Systems...
             Starting Remount Root and Kernel File Systems...
    [    4.534415] EXT4-fs (mmcblk1p2): re-mounted. Quota mode: none.
    [    4.554320] systemd[1]: Starting Coldplug All udev Devices...
             Starting Coldplug All udev Devices...
    [    4.588877] systemd[1]: Started Start psplash boot splash screen.
    [  OK  ] Started Start psplash boot splash screen.
    [    4.614150] systemd[1]: Started RPC Bind.
    [  OK  ] Started RPC Bind.
    [    4.634185] systemd[1]: Started Journal Service.
    [  OK  ] Started Journal Service.
    [  OK  ] Mounted Huge Pages File System.
    [  OK  ] Mounted POSIX Message Queue File System.
    [  OK  ] Mounted Kernel Debug File System.
    [  OK  ] Mounted Temporary Directory /tmp.
    [  OK  ] Finished Create List of Static Device Nodes.
    [  OK  ] Finished Load Kernel Module configfs.
    [  OK  ] Finished Load Kernel Module drm.
    [  OK  ] Finished Load Kernel Module fuse.
    [  OK  ] Finished Load Kernel Modules.
    [  OK  ] Finished Generate network units from Kernel command line.
    [  OK  ] Finished Remount Root and Kernel File Systems.
             Mounting FUSE Control File System...
             Mounting Kernel Configuration File System...
    [  OK  ] Started Start psplash-syst�progress communication helper.
             Starting Flush Journal to Persistent Storage...
             Starting Apply Kernel Variables...
    [    5.032941] systemd-journald[177]: Received client request to flush runtime journal.
             Starting Create Static Device Nodes in /dev...
    [  OK  ] Mounted FUSE Control File System.
    [  OK  ] Mounted Kernel Configuration File System.
    [  OK  ] Finished Flush Journal to Persistent Storage.
    [  OK  ] Finished Apply Kernel Variables.
    [  OK  ] Finished Create Static Device Nodes in /dev.
    [  OK  ] Reached target Preparation for Local File Systems.
             Mounting /media/ram...
             Mounting /var/volatile...
    [    5.255270] audit: type=1334 audit(1651167748.052:2): prog-id=5 op=LOAD
    [    5.262452] audit: type=1334 audit(1651167748.060:3): prog-id=6 op=LOAD
             Starting Rule-based Manage�for Device Events and Files...
    [  OK  ] Finished Coldplug All udev Devices.
    [  OK  ] Mounted /media/ram.
    [  OK  ] Mounted /var/volatile.
             Starting Load/Save Random Seed...
    [  OK  ] Reached target Local File Systems.
             Starting Create Volatile Files and Directories...
    [  OK  ] Finished Create Volatile Files and Directories.
             Starting Network Time Synchronization...
             Starting Record System Boot/Shutdown in UTMP...
    [  OK  ] Started Rule-based Manager for Device Events and Files.
    [  OK  ] Finished Record System Boot/Shutdown in UTMP.
    [  OK  ] Started Network Time Synchronizatio[    6.053571] random: crng init done
    n.
    [  OK  ] Finished Load/Save Random Seed.
    [  OK  ] Reached target System Initialization.
    [  OK  ] Started Daily Cleanup of Temporary [    6.117709] mc: Linux media interface: v0.10
    Directories.
    [  OK  ] Reached target System Time Set.
    [    6.142927] videodev: Linux video capture interface: v2.00
    [  OK  ] Started Daily rotation of log files.
    [  OK  ] Reached target Timer Units.
    [  OK  ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
    [  OK  ] Listening on D-Bus System Message Bus Socket.
             Starting Docker Socket for the API...[    6.248483] Bluetooth: Core ver 2.22
    
    [    6.253713] NET: Registered PF_BLUETOOTH protocol family
    [    6.259338] Bluetooth: HCI device and connection manager initialized
    [    6.267468] Bluetooth: HCI socket layer initialized
    [    6.276149] Bluetooth: L2CAP socket layer initialized
    [    6.282919] Bluetooth: SCO socket layer initialized
    [  OK  ] Listening on dropbear.socket.
    [  OK  ] Listening on PC/SC Smart Card Daemon Activation Socket.
    [    6.319773] btti serial0-0: Host wakeup NOT enabled
    [    6.343454] rtc-ti-k3 2b1f0000.rtc: registered as rtc0
    [    6.350045] rtc-ti-k3 2b1f0000.rtc: setting system clock to 1970-01-01T00:00:12 UTC (12)
             Starting Weston socket...
    [    6.387956] systemd-journald[177]: Time jumped backwards, rotating.
    [    6.390922] k3-m4-rproc 5000000.m4fss: assigned reserved memory node m4f-dma-memory@9cb00000
    [    6.409675] k3-m4-rproc 5000000.m4fss: configured M4 for remoteproc mode
             Starting Console System Startup Logging...
    [    6.435287] k3-m4-rproc 5000000.m4fss: local reset is deasserted for device
             Starting D-Bus System Message Bus...
    [    6.451351] remoteproc remoteproc0: 5000000.m4fss is available
             Starting Reboot and dump vmcore via kexec.[    6.471797] remoteproc remoteproc0: powering up 5000000.m4fss
    ..
    [    6.485078] remoteproc remoteproc0: Booting fw image am62-mcu-m4f0_0-fw, size 55016
    [    6.494907] rproc-virtio rproc-virtio.1.auto: assigned reserved memory node m4f-dma-memory@9cb00000
    [  OK  ] Listening on Docker Socket for the [    6.505515] rproc-virtio rproc-virtio.1.auto: registered virtio0 (type 7)
    API.
    [    6.517468] remoteproc remoteproc0: remote processor 5000000.m4fss is now up
    [  OK  ] Listening on Weston socket.
    [  OK  ] Finished Console System Startup Logging.
    [  OK  ] Finished Reboot and dump vmcore via kexec.
    [  OK  ] Found device /dev/ttyS2.
    [    6.594202] virtio_rpmsg_bus virtio0: rpmsg host is online
    [    6.602413] virtio_rpmsg_bus virtio0: creating channel ti.ipc4.ping-pong addr 0xd
    [  OK  ] Reached target Socket Units.
    [    6.642219] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0xe
    [    6.662986] sii902x 1-003b: supply iovcc not found, using dummy regulator
    [    6.673430] sii902x 1-003b: supply cvcc12 not found, using dummy regulator
    [    6.698796] i2c i2c-1: Added multiplexed i2c bus 3
    [    6.717651] platform 78000000.r5f: R5F core may have been powered on by a different host, programmed state (0) != actual state (1)
    [  OK  ] Started D-Bus System Message Bus    6.736867] [drm] Initialized tidss 1.0.0 20180215 for 30200000.dss on minor 0
    m.
    [    6.745124] platform 78000000.r5f: configured R5F for IPC-only mode
    [    6.752385] Console: switching 
    [    6.752403] platform 78000000.r5f: assigned reserved memory node r5f-dma-memory@9da00000
    [    6.752403] to colour dummy device 80x25
    [  OK  ] Reached target Basic System.
    [    6.775403] tidss 30200000.dss: [drm] Cannot find any crtc or sizes
    [    6.775543] remoteproc remoteproc1: 78000000.r5f is available
    [    6.794004] tidss 30200000.dss: [drm] Cannot find any crtc or sizes
    [    6.802082] remoteproc remoteproc1: attaching to 78000000.r5f
    [  OK  ] Started Job spooling tools.
    [    6.882777] platform 78000000.r5f: R5F core initialized in IPC-only mode
    [  OK  ] Started Periodic Command Scheduler.
             Starting DEMO...
             Starting Print notice about GPLv3 packages...
    [    6.959841] rproc-virtio rproc-virtio.3.auto: assigned reserved memory node r5f-dma-memory@9da00000
             Starting IPv6 Packet Filtering Framework...
             Starting IPv4 Packet Filtering Framework...
    [  OK  ] Started irqbalance daemon.
    [    7.007892] virtio_rpmsg_bus virtio1: rpmsg host is online
    [    7.018187] virtio_rpmsg_bus virtio1: creating channel ti.ipc4.ping-pong addr 0xd
    [    7.026694] virtio_rpmsg_bus virtio1: creating channel rpmsg_chrdev addr 0xe
    [    7.033853] rproc-virtio rproc-virtio.3.auto: registered virtio1 (type 7)
    [    7.033881] remoteproc remoteproc1: remote processor 78000000.r5f is now attached
    [    7.056697] cc33xx_sdio mmc2:0001:2: Using GPIO as IRQ
             Starting Telephony service...
             Starting PulseAudio Sound System...
             Starting Expand the rootfs…ll size of the boot device....
    [  OK  ] Started strongSwan IPsec I�IKEv2 daemon using ipsec.conf.
    [    7.173440] audit: type=1334 audit(13.320:4): prog-id=7 op=LOAD
    [    7.184329] audit: type=1334 audit(13.328:5): prog-id=8 op=LOAD
             Starting User Login Management...
    [  OK  ] Started TEE Supplicant.
             Starting Telnet Server...
    [  OK  ] Started ti-apps-launcher service.
    [  OK  ] Started DEMO.
    [  OK  ] Finished IPv6 Packet Filtering Framework.
    [  OK  ] Finished IPv4 Packet Filtering Framework.
    [  OK  ] Finished Telnet Server.
    [  OK  ] Started Telephony service.
    [  OK  ] Reached target Preparation for Network.
             Starting Network Configuration...
    [  OK  ] Started PulseAudio Sound System.
    [  OK  ] Finished Expand the rootfs�full size of the boot device..
    [  OK  ] Started User Login Management.
    [    8.204083] cfg80211: Loading compiled-in X.509 certificates for regulatory database
    [    8.238651] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
    [  OK  ] Started Network Configuration.
             Starting Network Name Resolution...
    [    8.416291] am65-cpsw-nuss 8000000.ethernet eth1: PHY [8000f00.mdio:01] driver [TI DP83867] (irq=POLL)
    [    8.425979] am65-cpsw-nuss 8000000.ethernet eth1: configuring for phy/rgmii-rxid link mode
    [    8.450037] am65-cpsw-nuss 8000000.ethernet eth0: PHY [8000f00.mdio:00] driver [TI DP83867] (irq=POLL)
    [    8.459507] am65-cpsw-nuss 8000000.ethernet eth0: configuring for phy/rgmii-rxid link mode
    [  OK  ] Listening on Load/Save RF �itch Status /dev/rfkill Watch.
    [    8.849524] remoteproc remoteproc2: 30074000.pru is available
    [    8.869799] remoteproc remoteproc3: 30078000.pru is available
    [    9.049717] tps6598x 0-003f: Unable to find the interrupt, switching to polling
    [    9.131404] cdns-csi2rx: probe of 30101000.csi-bridge failed with error -22
    [    9.257283] xhci-hcd xhci-hcd.5.auto: xHCI Host Controller
    [    9.268130] xhci-hcd xhci-hcd.5.auto: new USB bus registered, assigned bus number 1
    [  OK  ] Reached target Hardware activated U[    9.278527] xhci-hcd xhci-hcd.5.auto: USB3 root hub has no ports
    SB gadget.
    [    9.290624] xhci-hcd xhci-hcd.5.auto: hcc params 0x0258fe6d hci version 0x110 quirks 0x0000000000010010
    [    9.305727] xhci-hcd xhci-hcd.5.auto: irq 430, io mem 0x31100000
    [    9.327353] hub 1-0:1.0: USB hub found
    [    9.334798] hub 1-0:1.0: 1 port detected
    [  OK  ] Started Network Name Resolution.
    [  OK  ] Reached target Network.
    [  OK  ] Reached target Host and Network Name Lookups.
             Starting Avahi mDNS/DNS-SD Stack...
             Starting Enable and configure wl18xx bluetooth stack...
             Starting containerd container runtime...
    [  OK  ] Started Netperf Benchmark Server.
    [  OK  ] Started NFS status monitor for NFSv2/3 locking..
             Starting Simple Network Ma�ent Protocol (SNMP) Daemon....
             Starting Permit User Sessions...
    [  OK  ] Finished Enable and configure wl18xx bluetooth stack.
             Starting Save/Restore Sound Card State...
    [  OK  ] Finished Permit User Sessions.
    [  OK  ] Started Getty on tty1.
    [  OK  ] Started Serial Getty on ttyS2.
    [  OK  ] Reached target Login Prompts.
             Starting Synchronize System and HW clocks...
             Starting Weston, a Wayland�ositor, as a system service...
    [  OK  ] Started Avahi mDNS/DNS-SD Stack.
    [  OK  ] Finished Save/Restore Sound Card State.
    [  OK  ] Reached target Sound Card.
    [  OK  ] Created slice Slice /system/systemd-fsck.
    [    9.824189] audit: type=1334 audit(15.968:6): prog-id=9 op=LOAD
    [    9.830443] audit: type=1334 audit(15.976:7): prog-id=10 op=LOAD
             Starting User Database Manager...
    [  OK  ] Finished Synchronize System and HW clocks.
    [  OK  ] Found device /dev/mmcblk0p1.
             Starting File System Check on /dev/mmcblk0p1...
    [  OK  ] Finished File System Check on /dev/mmcblk0p1.
             Mounting /run/media/mmcblk0p1...
    [  OK  ] Started User Database Manager.
    [  OK  ] Mounted /run/media/mmcblk0p1.
    [  OK  ] Created slice User Slice of UID 1000.
             Starting User Runtime Directory /run/user/1000...
    [  OK  ] Finished User Runtime Directory /run/user/1000.
             Starting User Manager for UID 1000...
    [  OK  ] Started Simple Network Man�ement Protocol (SNMP) Daemon..
    [   10.412499] audit: type=1006 audit(16.556:8): pid=775 uid=0 old-auid=4294967295 auid=1000 tty=(none) old-ses=4294967295 ses=1 res=1
    [   10.425013] audit: type=1300 audit(16.556:8): arch=c00000b7 syscall=64 success=yes exit=4 a0=8 a1=ffffe8560908 a2=4 a3=ffff98da2020 items=0 ppid=1 pid=775 auid=1000 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=1 comm="(systemd)" exe="/lib/systemd/systemd" key=(null)
    [  OK  ] Found device /dev/mmcblk1p1.
    [   10.451238] audit: type=1327 audit(16.556:8): proctitle="(systemd)"
             Starting File System Check on /dev/mmcblk1p1...
    [  OK  ] Finished File System Check on /dev/mmcblk1p1.
             Mounting /run/media/boot-mmcblk1p1...
    [  OK  ] Mounted /run/media/boot-mmcblk1p1.
    [  OK  ] Started User Manager for UID 1000.
    [  OK  ] Started Session c1 of User weston.
    [   11.139031] audit: type=1006 audit(17.284:9): pid=700 uid=0 old-auid=4294967295 auid=1000 tty=tty7 old-ses=4294967295 ses=2 res=1
    [   11.150825] audit: type=1300 audit(17.284:9): arch=c00000b7 syscall=64 success=yes exit=4 a0=8 a1=ffffe8560908 a2=4 a3=ffff98da2020 items=0 ppid=1 pid=700 auid=1000 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=tty7 ses=2 comm="(weston)" exe="/lib/systemd/systemd" key=(null)
    [   11.176448] audit: type=1327 audit(17.284:9): proctitle="(weston)"
    [  OK  ] Started containerd container runtime.
    [   11.689119] wlcore: ERROR Device info command failure 
    [   11.694687] wlcore: ERROR FW download failed
    [  OK  ] Started Weston, a Wayland �mpositor, as a system service.
    ***************************************************************
    ***************************************************************
    NOTICE: This file system contains the following GPL-3.0 packages:
    	adwaita-icon-theme-symbolic
    	autoconf
    	bash-dev
    	bash
    	bc
    	binutils
    	cifs-utils
    	coreutils-stdbuf
    	coreutils
    	cpio
    	cpp-symlinks
    	cpp
    	dosfstools
    	elfutils
    	g++-symlinks
    	g++
    	gawk
    	gcc-symlinks
    	gcc
    	gdb
    	gdbserver
    	gettext
    	glmark2
    	gnu-config
    	grub-common
    	grub-editenv
    	grub-efi
    	gzip
    	hidapi
    	less
    	libasm1
    	libatomic-dev
    	libatomic1
    	libbfd
    	libdebuginfod1
    	libdw1
    	libeigen-dev
    	libelf1
    	libgcc-s-dev
    	libgcc1
    	libgdbm-compat4
    	libgdbm-dev
    	libgdbm6
    	libgettextlib
    	libgettextsrc
    	libgmp10
    	libidn2-0
    	libmpc3
    	libmpfr6
    	libopcodes
    	libqt5charts-examples
    	libqt5charts-plugins
    	libqt5charts-qmlplugins
    	libqt5charts5
    	libqt5sensors-plugins
    	libqt5sensors-qmlplugins
    	libqt5sensors5
    	libqt5serialport-examples
    	libqt5serialport-plugins
    	libqt5serialport-qmlplugins
    	libqt5serialport5
    	libqt5svg-examples
    	libqt5svg-plugins
    	libqt5svg-qmlplugins
    	libqt5svg5
    	libqt5virtualkeyboard-plugins
    	libqt5virtualkeyboard-qmlplugins
    	libqt5virtualkeyboard5
    	libqt5webchannel-plugins
    	libqt5webchannel-qmlplugins
    	libqt5webchannel5
    	libreadline-dev
    	libreadline8
    	libstdc++-dev
    	libstdc++6
    	libunistring2
    	m4-dev
    	m4
    	make
    	nettle
    	parted
    	piglit
    	qt3d-plugins
    	qt3d-qmlplugins
    	qt3d
    	qtbase-examples
    	qtbase-plugins
    	qtbase-qmlplugins
    	qtbase
    	qtconnectivity-plugins
    	qtconnectivity-qmlplugins
    	qtconnectivity
    	qtdeclarative-plugins
    	qtdeclarative-qmlplugins
    	qtdeclarative-tools
    	qtdeclarative
    	qtgraphicaleffects-qmlplugins
    	qtlocation-examples
    	qtlocation-plugins
    	qtlocation-qmlplugins
    	qtlocation
    	qtmultimedia-examples
    	qtmultimedia-plugins
    	qtmultimedia-qmlplugins
    	qtmultimedia
    	qtquick3d-plugins
    	qtquick3d-qmlplugins
    	qtquick3d
    	qtquics-qmlplugins.control
    	qtquics2-plugins.control
    	qtquics2-qmlplugins.control
    	qtquics2.control
    	qtscript-examples
    	qtscript-plugins
    	qtscript-qmlplugins
    	qtscript
    	qtwayland-examples
    	qtwayland-plugins
    	qtwayland-qmlplugins
    	qtwayland
    	tar
    	which
    
    If you do not wish to distribute GPL-3.0 components please remove
    the above packages prior to distribution.  This can be done using
    the opkg remove command.  i.e.:
        opkg remove <package>
    Where <package> is the name printed in the list above
    
    NOTE: If the package is a dependency of another package you
          will be notified of the dependent packages.  You should
          use the --force-removal-of-dependent-packages option to
          also remove the dependent packages as well
    ***************************************************************
    ***************************************************************
             Starting Wait for Network to be Configured...
    [  OK  ] Finished Print notice about GPLv3 packages.
    [  OK  ] Reached target Multi-User System.
    [  OK  ] Reached target Graphical Interface.
             Starting Record Runlevel Change in UTMP...
    [  OK  ] Finished Record Runlevel Change in UTMP.
    [   13.992643] sh (1192): drop_caches: 1
    
     _____                    _____           _         _   
    |  _  |___ ___ ___ ___   |  _  |___ ___  |_|___ ___| |_ 
    |     |  _| .'| . | . |  |   __|  _| . | | | -_|  _|  _|
    |__|__|_| |__,|_  |___|  |__|  |_| |___|_| |___|___|_|  
                  |___|                    |___|            
    
    Arago Project am62xx-evm -
    
    Arago 2023.10 am62xx-evm -
    
    am62xx-evm login: [   16.041034] ti-udma 485c0100.dma-controller: chan2 teardown timeout!
    
    am62xx-evm login: 
    am62xx-evm login: 
    am62xx-evm login: root
    [   19.923625] audit: type=1006 audit(26.068:10): pid=1210 uid=0 old-auid=4294967295 auid=0 tty=(none) old-ses=4294967295 ses=3 res=1
    [   19.935655] audit: type=1300 audit(26.068:10): arch=c00000b7 syscall=64 success=yes exit=1 a0=8 a1=ffffe8560908 a2=1 a3=ffff98da2020 items=0 ppid=1 pid=1210 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=3 comm="(systemd)" exe="/lib/systemd/systemd" key=(null)
    [   19.962422] audit: type=1327 audit(26.068:10): proctitle="(systemd)"
    [   19.969295] audit: type=1334 audit(26.108:11): prog-id=11 op=LOAD
    [   19.975454] audit: type=1300 audit(26.108:11): arch=c00000b7 syscall=280 success=yes exit=8 a0=5 a1=fffff0c92ab0 a2=78 a3=0 items=0 ppid=1 pid=1210 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=3 comm="systemd" exe="/lib/systemd/systemd" key=(null)
    [   20.000370] audit: type=1327 audit(26.108:11): proctitle="(systemd)"
    [   20.006914] audit: type=1334 audit(26.116:12): prog-id=11 op=UNLOAD
    [   20.013533] audit: type=1334 audit(26.116:13): prog-id=12 op=LOAD
    [   20.019710] audit: type=1300 audit(26.116:13): arch=c00000b7 syscall=280 success=yes exit=8 a0=5 a1=fffff0c92b50 a2=78 a3=0 items=0 ppid=1 pid=1210 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=3 comm="systemd" exe="/lib/systemd/systemd" key=(null)
    [   20.041064] ti-udma 485c0100.dma-controller: chan1 teardown timeout!
    [   20.044516] audit: type=1327 audit(26.116:13): proctitle="(systemd)"
    root@am62xx-evm:~# 
    root@am62xx-evm:~# 
    root@am62xx-evm:~# ls
    root@am62xx-evm:~# lsmod
    Module                  Size  Used by
    overlay               122880  0
    rpmsg_ctrl             16384  0
    cc33xx                274432  0
    rpmsg_char             16384  1 rpmsg_ctrl
    xhci_plat_hcd          16384  0
    mac80211              630784  1 cc33xx
    libarc4                16384  1 mac80211
    dwc3                   98304  1
    snd_soc_hdmi_codec     20480  0
    cdns_csi2rx            20480  0
    v4l2_fwnode            20480  1 cdns_csi2rx
    irq_pruss_intc         16384  0
    pru_rproc              24576  0
    cfg80211              385024  2 mac80211,cc33xx
    crct10dif_ce           16384  1
    snd_soc_simple_card    20480  0
    snd_soc_simple_card_utils    24576  1 snd_soc_simple_card
    cc33xx_sdio            16384  0
    display_connector      16384  0
    ti_k3_r5_remoteproc    28672  0
    virtio_rpmsg_bus       20480  0
    k3_j72xx_bandgap       16384  0
    rpmsg_ns               16384  1 virtio_rpmsg_bus
    dwc3_am62              16384  0
    ti_k3_m4_remoteproc    16384  0
    ti_k3_common           16384  1 ti_k3_m4_remoteproc
    rtc_ti_k3              16384  1
    btti_uart              20480  0
    j721e_csi2rx           24576  0
    bluetooth             548864  3 btti_uart
    videobuf2_dma_contig    20480  1 j721e_csi2rx
    rti_wdt                16384  0
    ecdh_generic           16384  1 bluetooth
    ecc                    36864  1 ecdh_generic
    rfkill                 24576  3 bluetooth,cfg80211
    videobuf2_memops       16384  1 videobuf2_dma_contig
    videobuf2_v4l2         32768  1 j721e_csi2rx
    sa2ul                  36864  0
    tidss                  61440  1
    cdns_dphy_rx           16384  0
    drm_dma_helper         20480  1 tidss
    videobuf2_common       57344  4 j721e_csi2rx,videobuf2_dma_contig,videobuf2_v4l2,videobuf2_memops
    v4l2_async             24576  3 v4l2_fwnode,j721e_csi2rx,cdns_csi2rx
    mcrc                   16384  0
    sii902x                20480  0
    snd_soc_tlv320aic3x_i2c    16384  1
    snd_soc_tlv320aic3x    77824  1 snd_soc_tlv320aic3x_i2c
    drm_kms_helper        184320  5 sii902x,drm_dma_helper,display_connector,tidss
    videodev              245760  5 v4l2_async,j721e_csi2rx,videobuf2_v4l2,cdns_csi2rx,videobuf2_common
    snd_soc_davinci_mcasp    32768  2
    tps6598x               20480  0
    syscopyarea            16384  1 drm_kms_helper
    sysfillrect            16384  1 drm_kms_helper
    snd_soc_ti_udma        16384  1 snd_soc_davinci_mcasp
    sysimgblt              16384  1 drm_kms_helper
    mc                     57344  6 v4l2_async,videodev,j721e_csi2rx,videobuf2_v4l2,cdns_csi2rx,videobuf2_common
    fb_sys_fops            16384  1 drm_kms_helper
    pruss                  16384  0
    snd_soc_ti_edma        16384  1 snd_soc_davinci_mcasp
    snd_soc_ti_sdma        16384  1 snd_soc_davinci_mcasp
    typec                  73728  1 tps6598x
    optee_rng              16384  0
    rng_core               20480  1 optee_rng
    fuse                  131072  1
    drm                   561152  7 sii902x,drm_kms_helper,drm_dma_helper,display_connector,tidss
    drm_panel_orientation_quirks    28672  1 drm
    ipv6                  475136  42
    root@am62xx-evm:~# dmesg | grep cc
    [    0.000000] Linux version 6.1.46-00001-g1e52556d77ab-dirty (fredy@ubuntu22-mini) (aarch64-oe-linux-gcc (GCC) 11.4.0, GNU ld (GNU Binutils) 2.38.20220708) #1 SMP PREEMPT Sat Jun 15 23:34:03 CST 2024
    [    0.000000] Reserved memory: created DMA memory pool at 0x000000009cc00000, size 14 MiB
    [    0.000000] OF: reserved mem: initialized node m4f-memory@9cc00000, compatible id shared-dma-pool
    [    1.430915] pca953x 1-0022: supply vcc not found, using dummy regulator
    [    6.662986] sii902x 1-003b: supply iovcc not found, using dummy regulator
    [    6.673430] sii902x 1-003b: supply cvcc12 not found, using dummy regulator
    [    7.056697] cc33xx_sdio mmc2:0001:2: Using GPIO as IRQ
    [    9.290624] xhci-hcd xhci-hcd.5.auto: hcc params 0x0258fe6d hci version 0x110 quirks 0x0000000000010010
    [    9.386387] wlcore: cc33xx_probe :: Start
    [   10.425013] audit: type=1300 audit(16.556:8): arch=c00000b7 syscall=64 success=yes exit=4 a0=8 a1=ffffe8560908 a2=4 a3=ffff98da2020 items=0 ppid=1 pid=775 auid=1000 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=1 comm="(systemd)" exe="/lib/systemd/systemd" key=(null)
    [   11.150825] audit: type=1300 audit(17.284:9): arch=c00000b7 syscall=64 success=yes exit=4 a0=8 a1=ffffe8560908 a2=4 a3=ffff98da2020 items=0 ppid=1 pid=700 auid=1000 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=tty7 ses=2 comm="(weston)" exe="/lib/systemd/systemd" key=(null)
    [   19.935655] audit: type=1300 audit(26.068:10): arch=c00000b7 syscall=64 success=yes exit=1 a0=8 a1=ffffe8560908 a2=1 a3=ffff98da2020 items=0 ppid=1 pid=1210 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=3 comm="(systemd)" exe="/lib/systemd/systemd" key=(null)
    [   19.975454] audit: type=1300 audit(26.108:11): arch=c00000b7 syscall=280 success=yes exit=8 a0=5 a1=fffff0c92ab0 a2=78 a3=0 items=0 ppid=1 pid=1210 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=3 comm="systemd" exe="/lib/systemd/systemd" key=(null)
    [   20.019710] audit: type=1300 audit(26.116:13): arch=c00000b7 syscall=280 success=yes exit=8 a0=5 a1=fffff0c92b50 a2=78 a3=0 items=0 ppid=1 pid=1210 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=3 comm="systemd" exe="/lib/systemd/systemd" key=(null)
    root@am62xx-evm:~# ifconfig
    eth0: flags=4099<UP,BROADCAST,MULTICAST>  mtu 1500
            ether 1c:63:49:22:50:18  txqueuelen 1000  (Ethernet)
            RX packets 0  bytes 0 (0.0 B)
            RX errors 0  dropped 0  overruns 0  frame 0
            TX packets 0  bytes 0 (0.0 B)
            TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0
    
    eth1: flags=4099<UP,BROADCAST,MULTICAST>  mtu 1500
            ether 70:ff:76:1e:d1:ac  txqueuelen 1000  (Ethernet)
            RX packets 0  bytes 0 (0.0 B)
            RX errors 0  dropped 0  overruns 0  frame 0
            TX packets 0  bytes 0 (0.0 B)
            TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0
    
    lo: flags=73<UP,LOOPBACK,RUNNING>  mtu 65536
            inet 127.0.0.1  netmask 255.0.0.0
            inet6 ::1  prefixlen 128  scopeid 0x10<host>
            loop  txqueuelen 1000  (Local Loopback)
            RX packets 94  bytes 7774 (7.5 KiB)
            RX errors 0  dropped 0  overruns 0  frame 0
            TX packets 94  bytes 7774 (7.5 KiB)
            TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0
    
    root@am62xx-evm:~# 
    root@am62xx-evm:~# no wn lan node here
    -sh: no: command not found
    root@am62xx-evm:~# pls hlep t     elp to check
    -sh: pls: command not found
    root@am62xx-evm:~# 

    Regards,

    Fredy Zhang 

  • Hi Fredy,

    I don't see anything wrong with the log but there could be a potential hardware issue. Can you provide the entire name of the M2 - CC3301, as in is it the E1 or the E2 version?

    Secondly, were you able to solder on the R6 resistor? Please refer to the Linux user guide SK-AM62B-P1 and M2-CC3301 section for detailed instructions. 

    Warm regards,

    Christina

  • Christina, 

    I didn't have R6 on the board. and M2-CC3301 MCU126E1 Version.  Let me if you have any other comments.

    Regards,

    Fredy Zhang 

  • Hi Fredy,

    Apologies for any confusion. Since you have the E1 revision, the R6 resistor needs to be removed. Also, you will need to configure the IRQ for the M2-CC3301 E1 board to IRQ_TYPE_EDGE_RISING like so in the k3-am625-sk.dts

    #address-cells = <1>;
    	#size-cells = <0>;
    	wlcore: wlcore@2 {
    		compatible = "ti,cc33xx";
    		reg = <2>;
    		pinctrl-names = "default";
    		pinctrl-0 = <&main_wlirq_pins_default>;
    		interrupt-parent = <&main_gpio0>;
    		interrupts = <72 IRQ_TYPE_EDGE_RISING>;
    	};

    We strongly recommend getting a new M.2 card with the E2, instead of getting it to work as we do not support the E1 anymore. 

    BR. 

    Christina