Part Number: CC3301MOD
Other Parts Discussed in Thread: CC3301, LP-AM243, UNIFLASH
I have got he BP-CC3301MOD & LP-AM243 for Evaluating the Wi-Fi Features on CC3301 Wi-Fi Module
I have build the below output image using the cc33xx_rtos_mcu_package_R8 SDK.
cc3xxx_network_terminal/build_cc3xx_release/cc3xxx_network_terminal.appimage
As per the Programming Instructions in CC33XX MCU User Guide
Set the Uart Boot Mode
Added all the binary file path in program_application_and_wifi_fw.cfg
Executed the Script py uart_uniflash.py -p COM4 --cfg=program_application_and_wifi_fw.cfg
I am getting error while the 2nd commad in the script is executed i.e for below operation
Program the OSPI PHY tuning attack vector
--operation=flash-phy-tuning-data
send error: expected NAK, CRC, EOT or CAN; got b'2'
PFA screenhot of the Error & the Eval Board .
Kindly request to help resolve this issue.