Part Number: CC3235MODSF
Hi
We want to scan the specific AP only which is set to hidden SSID, so we want to know how to modify the code to scan the specific AP only with hidden SSID.
We are currently using Network Terminal Example and developing our product.
Before making Wi-Fi connection, we want to know if the specific AP is within the range by scanning, even though it is set to hidden SSID.
After the specific AP with hidden SSID is scanned correctly, then we want to make Wi-Fi connection.
But, in the Network Terminal example when we run the scan after the scan policy set, we are not able to see "SSID", because AP is set to hidden SSID
And, we do not know if the scanned AP is the one what we want to connnect to or something else?
My question is ;
1. when AP is set to hidden SSID and scan the specific SSID only, is it possible to get the scan result with SSID?
(for example. giving "scan RJNEOBD_999995 -n 30 EXT" command, can I see RJNEOBD_99995 in the scan result?)
2. to scan the specific SSID only, which one I need to modify ?
(in Network Terminal Example, to scan the specific SSID only ( like scan SSID -n 30 EXT) which one and how to modify the current example?)
Here is the log when run the scan enabling hidden SSID in Network Terminal Example.
setpolicy -i 30 -h YES
scan -n 30 EXT
----------------------------------------------------------------------------------------------------------------
| SSID | BSSID | RSSI | Ch | Hidden | Security | Country Code | 2.4gHz Channels | 5Ghz Channels|
----------------------------------------------------------------------------------------------------------------
16 | DSCAN-TESTIM25 | b2:38:6c:49:c6:8c | -73 | 36 | NO | WPA2 | KR | 0x0000 | 0x1ffffff |
17 | mac | c8:03:f5:77:7c:cc | -94 | 40 | NO | OPEN | KR | 0x0000 | 0x000f |
18 | deepbio_bd | c8:03:f5:b7:7c:cc | -93 | 40 | NO | OPEN | KR | 0x0000 | 0x000f |
19 | deepbio_mobile | c8:03:f5:37:7c:cd | -94 | 40 | NO | OPEN | KR | 0x0000 | 0x000f |
20 | deepbio_test | c8:03:f5:37:7c:cc | -93 | 40 | NO | WPA2 | KR | 0x0000 | 0x000f |
21 | | 88:1a:14:c7:7a:b4 | -77 | 48 | YES | OPEN | 0 | 0x0000 | 0x0000 | <= ssid RJNEOBD_999995
Thanks