Good day,
I've downloaded/installed both IAR Workbench and CCSv5 and I'm trying to build and run the basic WiFi app on my MSP430 Fram experimentors board with CC3000 TiWi module but I get errors from both programs when I try to build:
From CCSv5 when I try to build BasicWiFiApplication:
From IAR when I try to make BasicWiFiApplication:
[Og007]: Assembler list file generation not allowed in this version of the compiler
Error while running C/C++ compiler
board.c
[Og007]: Assembler list file generation not allowed in this version of the compiler
Error while running C/C++ compiler
Can anyone help me? Please
I am using version 5.51.6 of IAR workbench for MSP430
I read that there where some linking errors in another post on this forum. But when I click project > there is no properties button to click ? I cant find where to change the symbolic links. Please could some one help me. I dono if i maybe have a newer version of workbench or what. But there should still be a properties button some where i have looked and i cant find one.
If I click on project i only get an options button that gives me a different interface.
I am not sure what i am doing wrong. But i am quite certain it has to do some thing with the source code or my setup of the ide., But i find it odd that i get errors on two ides.