Hi I'm trying to get the MSP430 Launchpad to connect with the CC3000 using the Smart Connect feature.
Right now I'm following the guide below to configure the CC3000 and got to the Terminal outputting the "Example App: drive version 2......" text.
Now when I try to enter the command "01" so I can start the Smart Connect, I don't get a echo or replay back from the CC3000. It just sits there and lets me continuously enter keys but nothing will show up on the Terminals.
Does anybody happen to know why this is? I've patched the CC3000 to the lastest firmware and the LEDs on the MSP430 are lit up after patching.
I'm running CCS v5.4 and using Tera Terminal if that matters.
Thanks, Joey