I am working AM335x EVM + WL1833 module.
I am developing WL1833 module and it's pin compatable with COM8 WL1835.
I tested already its operation of Linux OS using ti-sdk-am335x-evm-06.00.00.00 and it is working well.
But Bluetooth is not working in android JB 4.2.2.
I have built according to following link.
http://processors.wiki.ti.com/index.php/TI-Android-JB-4.2.2-DevKit-4.1.1_DeveloperGuide
I downloaded source from row-boat gitorious and builded.
WiFi STA mode worked well in both 2.4GHz and 5GHz.
But When I turn on BT in settings, it turns off right away.
And sometimes, During BT pairing processing, I can find BT pairing device name on AM335x EVM, but it can't be used.
TI pre-built image(Android-NLCP, ol_R8.A6.02) is same result.
http://processors.wiki.ti.com/index.php/WL8_release_download_page#Demo_Release
And what's the meaning of N.C of BT tab in Android_4_2.xlsx file linked in Test Result?
In JB4.2.2, Do AM335x EVM + WL1833 operate corectly BT?
Refer blow message for BT malfunction.
message..
[ 36.617706] (hci_tty): inside hci_tty_open (de03e648, cf0a76c0)
[ 54.213287] (hci_tty): inside hci_tty_release (de03e648, cf0a76c0)
[ 60.694915] (hci_tty): inside hci_tty_open (de03e648, db0846c0)
[ 62.062408] (stk) :response timeout during fw download
[ 62.067810] (stk) :download firmware failed
[ 63.442382] (stk) :response timeout during fw download
[ 63.447753] (stk) :download firmware failed
[ 64.822387] (stk) :response timeout during fw download
[ 64.827789] (stk) :download firmware failed
[ 66.202392] (stk) :response timeout during fw download
[ 66.207794] (stk) :download firmware failed
[ 67.582397] (stk) :response timeout during fw download
[ 67.587799] (stk) :download firmware failed
[ 68.962554] (stk) :response timeout during fw download
[ 68.967987] (stk) :download firmware failed
[ 68.973693] (hci_tty): st_register failed -22