This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3000 API wlan_connect function / HCI_CMND_WLAN_CONNECT (opcode 0x0001) SSID field limited to 30 characters?



While experimenting with CC3000 wlan_connect (and underlying HCI_CMND_WLAN_CONNECT command), I did not manage to associate CC3000 with an access point if the SSID field was longer than 30 bytes.

The SSID field can typically be 1 to 32 characters long, also the CC3000 API documentation says up to 32 bytes should be accepted.

After issuing wlan_connect with 31 or 32 char long SSID's, I experienced CC3000 to go into a non-normal state, where it even after power cycling could not connect to any APs anymore (incl. also short SSIDs). First after rewriting the NVMEM/EEPROM with PatchProgrammers DR and FW, I was able to regain normal operation.

Has anyone experienced or could possibly verify this behavior?

Thanks,
Risto