Other Parts Discussed in Thread: CC3100
All,
I cant seem to get UDP sockets to work at all using the new FW version 1.13. Anybody else see this too? I am getting the correct response to sendto after opening and binding the socket, but the cc3000 locks up and does not respond after sending the correct response back. I am not getting the data to actually be broadcast by the CC3000, either.
I am having the same trouble with the MDNS advertise which is also built on udp. I can continually try to send MDNS but nothing is ever broadcast by the CC3000. I get the correct response and can move on afterwards but it still doesn't work. Maybe it is not locking up the CC3000 because it is an unbound UDP socket?
Am I missing something that changed drastically with either of these in version 1.12.0.
TI do we use the same API for 1.12 and 1.13? And by the way what is changed to "uint8" in mdsn advertise? ->
| Network | In nvmem_create_entry(), mdnsAdvertiser(), changing “int” to “TO_UINT8” |
In the api I only see uint16 for mdns advertise.
It seems everything else works so far with smart config and joining an AP and even with TCP so I am really hoping I am missing something.
Thanks,
Chad