I want to establish a UART connection from the Launchpad EK-TM4C123GXL+ CC3100 booster pack to another MCU, the LM3S811 M3. The connections will run from the Launchpad to the LM3S811 that is soldered to board. My question is regarding available UART communication between the Launchpad TM4C and the LM3S811.
These are the available UARTs I researched for the Launchpad + CC3100:
CC3100 Task | UART |
WLAN_LOG_TX | UART2_Rx |
NC | UART2_Tx |
NC | UART3_Rx |
NWP_LOG_TX | UART3_Tx |
nHIB | UART5 |
UNUSED | UART5 |
SPI_CS | UART7_Rx |
NC | UART7_Tx |
Our options we are considering:
1. Use UART2_Tx and UART3_Rx or
2. Use UART2_Tx and UART2_Rx by overriding/disabling WLAN_LOG_TX functionality on UART2_Rx
Questions:
1. Can we use a Tx and Rx line that are on two separate UARTs?
2. Or, can we not use WLAN_LOG_TX and use it for our Rx line?
Also, can we expect to have any issues transferring the incoming wifi data across the UART line to the LM3S811?
Thanks!