Other Parts Discussed in Thread: CC3100, MSP430F5529
hello!
i have just recieved two cc3100 boosterpacks and two cc3100 advanced emulation boosterpcaks for my project. i have tried some of the example applications availble with the sdk and now ready to go to the next stage.
I'm trying to set up a wifi expirement between two cc3100 boosterpacks (each connected to a boosterpcak emulator which is connected to a pc). my aim is to send data from one unit to another using a LAN, during the experiment i will be evaluating the range and speed of data transfer.
1. is there any already written example project i can use?
2. if the anwser to the first question is "no", what should i do in order to make progress?
thanks :)