In the user guide I see that in order to program the serial flash in the CC3100MOD or if we will use the CC3100, it needs to be done using the UART interface?
or it can be done from the SPI also.
we plan to connect the CC3100MOD to the MSP430F5521 via the SPI interface only. can we program the serial Flash using the SPI or we need UART connection as well?