Hello,
I designed some board using CC3200 refrenced from evaluation board schematic. Our schematic is attached. There is no signal in the 32kHz and 40MHz crystal after power up. I can see the clk from evaluation board at the same condition. I don't know what is the problem. Pls see our schematic attached if there are some missing point.
Thanks, SebeomWDL3000 _ 01.pdf