Hello,
We are trying to run the CC3100 using a STM32F207 as the controlling processor. Unfortunately we are running into some issues with porting the CC3100 SDK functions over to the STM processor.
Some notes:
- The Inhibit pin is pulled high with pin processor pin to control it.
- We are using SPI to communicate with the CC3100
- The CC3100 firmware is placed in its own thread at the begining.
The first issue we are running into is a memory overflow when we use the vSimpleLinkSpawnTask( ) and osi_Spawn() functions in osi_freertos.c to handle passing our semaphores. After a single successful interaction between the CC3100 and the processor, the Queue pointed at by SimpleLinkSpawnQueue variable has been overwritten with incorrect data. Most notably the uxItemSize variable in the Queue has been set to a pointer value, so when the Queue re-enters the xQueueReceive it does a memcpy of a pointer value (0x200062d8)... which of course causes a lot more problems.
I noticed some issues with pointers in the SDK examples with regards to the user.h Multithreaded defines, but the functions from the osi_freertos.c seems to have resolved the issues I noticed. I attempted to track this down myself, but was unfortunately unable to find a location in the Spawn Thread. I noticed it seemed to happen in a debug sprintf (fine before... overwritten after), but removing this statement had no effect (and the destination pointer was located after the memory location getting overwritten), thus I believe it might be occurring in another thread or an interrupt. For a further test, if I bypass the osi_Spawn() function and instead set the sl_Spawn define to sl_SyncObjSignalFromIRQ(&g_pCB->ObjPool[0].SyncObj) in order to directly set the semaphore that sl_Start is waiting for, the process continues and I'm able to begin to talk to the CC3100.
Any idea where this Queue's data could be overwritten, seems like a faulty pointer somewhere... but I'm not able to located it, so if anyone has run into something similar before, I'd appreciate a nudge in the right direction.
My second issue involves the actual communication with the CC3100. I try to set it to AP mode and proceed to get communication back and forth as expected, until I reach the end of the communication. The CC3100 functions are waiting for an RECV_RESP_CLASS message but it never arrives, so the communication eventually times out even though it has been talking and has given me a IP address. One thing I am concerned about is the response Sync bytes are not quite what I expected. All the documentation I've seen says it should be 0xABCDDCBA, however I get 0xABCDDCBC. This sync byte still passes the N2H_SYNC_PATTERN_MATCH and proceeds to continue to communicate. See below for the output from console for the communications:
WifiManager is up! SM=0
Configuring to Station mode
_SlDrvDriverCBInit done!
_SlDrvCmdOp: call _SlDrvMsgWrite
SPI write
WIFI_Manager: 21433412
SPI write
WIFI_Manager: B48C0400
Descriptor
SPI write
WIFI_Manager: 00A5A5A5
_SlDrvCmdOp: call _SlDrvMsgReadCmdCtx
_SlDrvMsgReadCmdCtx: Waiting for resp 1 == 0
_SlDrvMsgRead
SPI write
WIFI_Manager: 65877856
SPI Read
WIFI_Manager: BCDCCDAB08000800
SPI Read
WIFI_Manager:
Rx Sync: op=0008 len=0008
SPI Read
WIFI_Manager: 00000000
WIFI_Manager: 0800080000000000
_SlDrvMsgRead: op=0008, PL-len=0004
SPI Read
WIFI_Manager: 33333333
_SlDrvMsgRead: RspLen=0004 LenRx=0004
_SlDrvMsgReadCmdCtx - 1
_SlDrvMsgReadCmdCtx: Waiting for resp 2 == 1
_SlDrvMsgRead
SPI write
WIFI_Manager: 65877856
SPI Read
WIFI_Manager: BDDCCDAB25181000
SPI Read
WIFI_Manager:
Rx Sync: op=1825 len=0010
SPI Read
WIFI_Manager: 38000000
WIFI_Manager: 2518100038000000
_SlDrvMsgRead: op=1825, PL-len=000c
SPI Read
WIFI_Manager: 0101A8C00101A8C000000000
_SlDrvMsgRead: RspLen=000c LenRx=000c
[NETAPP EVENT] IP ACQUIRED
_SlDrvMsgReadCmdCtx - 1
_SlDrvMsgReadCmdCtx: Waiting for resp 2 == 2
_SlDrvMsgReadCmdCtx - 2
_SlDrvMsgReadCmdCtx: Waiting for resp 2 == 2
_SlDrvMsgReadCmdCtx - 2
_SlDriverHandleError
[GENERAL EVENT]
Note the output only converts each byte into ASCII at a time, thus 0x21433412 as seen in the output is actually 0x12344321.
Again I'm at a bit of a loss as to why the processor never receives the expected response in order to not time out. Any ideas?
Since the main setup for using the CC3100 SDK functions is the user.h file, I have attached it... perhaps I have overlooked something? If there is any other information needed, let me know.
Thanks,
Davin Morris
/* * user.h - CC31xx/CC32xx Host Driver Implementation * * Copyright (C) 2014 Texas Instruments Incorporated - http://www.ti.com/ * * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the * distribution. * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * */ #ifndef __USER_H__ #define __USER_H__ #ifdef __cplusplus extern "C" { #endif /*! \addtogroup Porting @{ */ /*! ****************************************************************************** \defgroup porting_user_include User Include Files This section IS NOT REQUIRED in case user provided primitives are handled in makefiles or project configurations (IDE) PORTING ACTION: - Include all required header files for the definition of: -# Transport layer library API (e.g. SPI, UART) -# OS primitives definitions (e.g. Task spawn, Semaphores) -# Memory management primitives (e.g. alloc, free) in order to "install" external SimpleLink library one should follow the next steps: 1. Include the external library API header file (i.e. #include "IOT.h") 2. Define each one of the desired external lib with one (out of 5) of the following: #define SL_EXT_LIB_1 <Your external lib name> #define SL_EXT_LIB_2 <Your external lib name> #define SL_EXT_LIB_3 <Your external lib name> #define SL_EXT_LIB_4 <Your external lib name> #define SL_EXT_LIB_5 <Your external lib name> ****************************************************************************** */ #include "wifidrv.h" #include "string.h" #include "memmgr.h" #include "osi.h" #define SL_SMALL /*! ****************************************************************************** \defgroup porting_capabilities Capability Set Definition This section IS NOT REQUIRED in case one of the following pre defined capabilities set is in use: - SL_TINY - SL_SMALL - SL_FULL PORTING ACTION: - Define one of the pre-defined capabilities set or uncomment the relevant definitions below to select the required capabilities @{ ******************************************************************************* */ /*! \def MAX_CONCURRENT_ACTIONS \brief Defines the maximum number of concurrent action in the system Min:1 , Max: 32 Actions which has async events as return, can be \sa \note In case there are not enough resources for the actions needed in the system, error is received: POOL_IS_EMPTY one option is to increase MAX_CONCURRENT_ACTIONS (improves performance but results in memory consumption) Other option is to call the API later (decrease performance) \warning In case of setting to one, recommend to use non-blocking recv\recvfrom to allow multiple socket recv */ #ifndef SL_TINY_EXT #define MAX_CONCURRENT_ACTIONS 10 #else #define MAX_CONCURRENT_ACTIONS 1 #endif /*! \def CPU_FREQ_IN_MHZ \brief Defines CPU frequency for Host side, for better accuracy of busy loops, if any \sa \note \warning If not set the default CPU frequency is set to 200MHz This option will be deprecated in future release */ /* #define CPU_FREQ_IN_MHZ 25 */ /*! \def SL_INC_ARG_CHECK \brief Defines whether the SimpleLink driver perform argument check or not When defined, the SimpleLink driver perform argument check on function call. Removing this define could reduce some code size and improve slightly the performances but may impact in unpredictable behaviour in case of invalid arguments \sa \note belongs to \ref porting_sec \warning Removing argument check may cause unpredictable behaviour in case of invalid arguments. In this case the user is responsible to argument validity (for example all handlers must not be NULL) */ #define SL_INC_ARG_CHECK /*! \def SL_INC_STD_BSD_API_NAMING \brief Defines whether SimpleLink driver should expose standard BSD APIs or not When defined, the SimpleLink driver in addition to its alternative BSD APIs expose also standard BSD APIs. Standard BSD API includes the following functions: socket , close , accept , bind , listen , connect , select , setsockopt , getsockopt , recv , recvfrom , write , send , sendto , gethostbyname \sa \note belongs to \ref porting_sec \warning */ #define SL_INC_STD_BSD_API_NAMING /*! \brief Defines whether to include extended API in SimpleLink driver or not When defined, the SimpleLink driver will include also all extended API of the included packages \sa ext_api \note belongs to \ref porting_sec \warning */ #define SL_INC_EXT_API /*! \brief Defines whether to include WLAN package in SimpleLink driver or not When defined, the SimpleLink driver will include also the WLAN package \sa \note belongs to \ref porting_sec \warning */ #define SL_INC_WLAN_PKG /*! \brief Defines whether to include SOCKET package in SimpleLink driver or not When defined, the SimpleLink driver will include also the SOCKET package \sa \note belongs to \ref porting_sec \warning */ #define SL_INC_SOCKET_PKG /*! \brief Defines whether to include NET_APP package in SimpleLink driver or not When defined, the SimpleLink driver will include also the NET_APP package \sa \note belongs to \ref porting_sec \warning */ #define SL_INC_NET_APP_PKG /*! \brief Defines whether to include NET_CFG package in SimpleLink driver or not When defined, the SimpleLink driver will include also the NET_CFG package \sa \note belongs to \ref porting_sec \warning */ #define SL_INC_NET_CFG_PKG /*! \brief Defines whether to include NVMEM package in SimpleLink driver or not When defined, the SimpleLink driver will include also the NVMEM package \sa \note belongs to \ref porting_sec \warning */ #define SL_INC_NVMEM_PKG /*! \brief Defines whether to include socket server side APIs in SimpleLink driver or not When defined, the SimpleLink driver will include also socket server side APIs \sa server_side \note \warning */ #define SL_INC_SOCK_SERVER_SIDE_API /*! \brief Defines whether to include socket client side APIs in SimpleLink driver or not When defined, the SimpleLink driver will include also socket client side APIs \sa client_side \note belongs to \ref porting_sec \warning */ #define SL_INC_SOCK_CLIENT_SIDE_API /*! \brief Defines whether to include socket receive APIs in SimpleLink driver or not When defined, the SimpleLink driver will include also socket receive side APIs \sa recv_api \note belongs to \ref porting_sec \warning */ #define SL_INC_SOCK_RECV_API /*! \brief Defines whether to include socket send APIs in SimpleLink driver or not When defined, the SimpleLink driver will include also socket send side APIs \sa send_api \note belongs to \ref porting_sec \warning */ #define SL_INC_SOCK_SEND_API /*! Close the Doxygen group. @} */ /*! ****************************************************************************** \defgroup porting_enable_device Device Enable/Disable IO The enable/disable API provide mechanism to enable/disable the network processor PORTING ACTION: - None @{ ****************************************************************************** */ /*! \brief Preamble to the enabling the Network Processor. Placeholder to implement any pre-process operations before enabling networking operations. \sa sl_DeviceEnable \note belongs to \ref ported_sec */ #define sl_DeviceEnablePreamble() /*! \brief Enable the Network Processor \sa sl_DeviceDisable \note belongs to \ref porting_sec */ #define sl_DeviceEnable() HAL_GPIO_WritePin(nRF_RST_GPIO_Port, nRF_RST_Pin, GPIO_PIN_SET) //#define sl_DeviceEnable() /*! \brief Disable the Network Processor \sa sl_DeviceEnable \note belongs to \ref porting_sec */ #define sl_DeviceDisable() HAL_GPIO_WritePin(nRF_RST_GPIO_Port, nRF_RST_Pin, GPIO_PIN_RESET) //#define sl_DeviceDisable() /*! Close the Doxygen group. @} */ /*! ****************************************************************************** \defgroup porting_interface Hardware Transport Interface The simple link device can work with different transport interfaces (namely,SPI or UART). Texas Instruments provides single driver that can work with all these types. This section binds the physical transport interface with the SimpleLink driver \note Correct and efficient implementation of this driver is critical for the performances of the SimpleLink device on this platform. PORTING ACTION: - None @{ ****************************************************************************** */ #define _SlFd_t short* /*! \brief Opens an interface communication port to be used for communicating with a SimpleLink device Given an interface name and option flags, this function opens the communication port and creates a file descriptor. This file descriptor is used afterwards to read and write data from and to this specific communication channel. The speed, clock polarity, clock phase, chip select and all other specific attributes of the channel are all should be set to hardcoded in this function. \param ifName - points to the interface name/path. The interface name is an optional attributes that the simple link driver receives on opening the driver (sl_Start). In systems that the spi channel is not implemented as part of the OS device drivers, this parameter could be NULL. \param flags - optional flags parameters for future use \return upon successful completion, the function shall open the channel and return a non-negative integer representing the file descriptor. Otherwise, -1 shall be returned \sa sl_IfClose , sl_IfRead , sl_IfWrite \note The prototype of the function is as follow: Fd_t xxx_IfOpen(char* pIfName , unsigned long flags); \note belongs to \ref porting_sec \warning */ #define sl_IfOpen WifiDrv_Open /*! \brief Closes an opened interface communication port \param fd - file descriptor of opened communication channel \return 0 - successful -1 - fail \sa sl_IfOpen , sl_IfRead , sl_IfWrite \note The prototype of the function is as follow: int xxx_IfClose(Fd_t Fd); \note belongs to \ref porting_sec \warning */ #define sl_IfClose WifiDrv_Close /*! \brief Attempts to read up to len bytes from an opened communication channel into a buffer starting at pBuff. \param fd - file descriptor of an opened communication channel \param pBuff - pointer to the first location of a buffer that contains enough space for all expected data \param len - number of bytes to read from the communication channel \return upon successful completion, the function shall return the number of read bytes. Otherwise, 0 shall be returned \sa sl_IfClose , sl_IfOpen , sl_IfWrite \note The prototype of the function is as follow: int xxx_IfRead(Fd_t Fd , char* pBuff , int Len); \note belongs to \ref porting_sec \warning */ #define sl_IfRead WifiDrv_Read /*! \brief attempts to write up to len bytes to the SPI channel \param fd - file descriptor of an opened communication channel \param pBuff - pointer to the first location of a buffer that contains the data to send over the communication channel \param len - number of bytes to write to the communication channel \return upon successful completion, the function shall return the number of sent bytes. otherwise, 0 shall be returned \sa sl_IfClose , sl_IfOpen , sl_IfRead \note This function could be implemented as zero copy and return only upon successful completion of writing the whole buffer, but in cases that memory allocation is not too tight, the function could copy the data to internal buffer, return back and complete the write in parallel to other activities as long as the other SPI activities would be blocked until the entire buffer write would be completed The prototype of the function is as follow: int xxx_IfWrite(Fd_t Fd , char* pBuff , int Len); \note belongs to \ref porting_sec \warning */ #define sl_IfWrite WifiDrv_Write /*! \brief register an interrupt handler routine for the host IRQ \param InterruptHdl - pointer to interrupt handler routine \param pValue - pointer to a memory structure that is passed to the interrupt handler. \return upon successful registration, the function shall return 0. Otherwise, -1 shall be returned \sa \note If there is already registered interrupt handler, the function should overwrite the old handler with the new one \note If the handler is a null pointer, the function should un-register the interrupt handler, and the interrupts can be disabled. \note belongs to \ref porting_sec \warning */ #define sl_IfRegIntHdlr(InterruptHdl , pValue) //#define sl_IfRegIntHdlr(InterruptHdl , pValue) WifiDrv_RegisterIRQHandler(InterruptHdl , pValue) /*! \brief Masks the Host IRQ \sa sl_IfUnMaskIntHdlr \note belongs to \ref porting_sec \warning */ #define sl_IfMaskIntHdlr() WifiDrvMaskIRQ() /*! \brief Unmasks the Host IRQ \sa sl_IfMaskIntHdlr \note belongs to \ref porting_sec \warning */ #define sl_IfUnMaskIntHdlr() WifiDrvUnmaskIRQ() /*! \brief Write Handers for statistics debug on write \param interface handler - pointer to interrupt handler routine \return no return value \sa \note An optional hooks for monitoring before and after write info \note belongs to \ref porting_sec \warning */ /* #define SL_START_WRITE_STAT */ #ifdef SL_START_WRITE_STAT #define sl_IfStartWriteSequence #define sl_IfEndWriteSequence #endif /*! Close the Doxygen group. @} */ /*! ****************************************************************************** \defgroup porting_mem_mgm Memory Management This section declare in which memory management model the SimpleLink driver will run: -# Static -# Dynamic This section IS NOT REQUIRED in case Static model is selected. The default memory model is Static PORTING ACTION: - If dynamic model is selected, define the alloc and free functions. @{ ***************************************************************************** */ /*! \brief Defines whether the SimpleLink driver is working in dynamic memory model or not When defined, the SimpleLink driver use dynamic allocations if dynamic allocation is selected malloc and free functions must be retrieved \sa \note belongs to \ref porting_sec \warning */ #define SL_MEMORY_MGMT_DYNAMIC #ifdef SL_MEMORY_MGMT_DYNAMIC /*! \brief \sa \note belongs to \ref porting_sec \warning */ #define sl_Malloc(Size) MemAlloc(Size) /*! \brief \sa \note belongs to \ref porting_sec \warning */ #define sl_Free(pMem) MemFree(pMem) #endif /*! Close the Doxygen group. @} */ /*! ****************************************************************************** \defgroup porting_os Operating System (OS) The simple link driver can run on multi-threaded environment as well as non-os environment (main loop) This section IS NOT REQUIRED in case you are working on non-os environment. If you choose to work in multi-threaded environment under any operating system you will have to provide some basic adaptation routines to allow the driver to protect access to resources from different threads (locking object) and to allow synchronization between threads (sync objects). PORTING ACTION: -# Uncomment SL_PLATFORM_MULTI_THREADED define -# Bind locking object routines -# Bind synchronization object routines -# Optional - Bind spawn thread routine @{ ****************************************************************************** */ #define SL_PLATFORM_MULTI_THREADED #ifdef SL_PLATFORM_MULTI_THREADED /*! \brief \sa \note belongs to \ref porting_sec \warning */ #define SL_OS_RET_CODE_OK ((int)OSI_OK) /*! \brief \sa \note belongs to \ref porting_sec \warning */ #define SL_OS_WAIT_FOREVER ((OsiTime_t)OSI_WAIT_FOREVER) /*! \brief \sa \note belongs to \ref porting_sec \warning */ #define SL_OS_NO_WAIT ((OsiTime_t)OSI_NO_WAIT) /*! \brief type definition for a time value \note On each porting or platform the type could be whatever is needed - integer, pointer to structure etc. \note belongs to \ref porting_sec */ #define _SlTime_t OsiTime_t /*! \brief type definition for a sync object container Sync object is object used to synchronize between two threads or thread and interrupt handler. One thread is waiting on the object and the other thread send a signal, which then release the waiting thread. The signal must be able to be sent from interrupt context. This object is generally implemented by binary semaphore or events. \note On each porting or platform the type could be whatever is needed - integer, structure etc. \note belongs to \ref porting_sec */ #define _SlSyncObj_t OsiSyncObj_t /*! \brief This function creates a sync object The sync object is used for synchronization between different thread or ISR and a thread. \param pSyncObj - pointer to the sync object control block \return upon successful creation the function should return 0 Otherwise, a negative value indicating the error code shall be returned \note belongs to \ref porting_sec \warning */ #define sl_SyncObjCreate(pSyncObj,pName) osi_SyncObjCreate(pSyncObj) /*! \brief This function deletes a sync object \param pSyncObj - pointer to the sync object control block \return upon successful deletion the function should return 0 Otherwise, a negative value indicating the error code shall be returned \note belongs to \ref porting_sec \warning */ #define sl_SyncObjDelete(pSyncObj) osi_SyncObjDelete(pSyncObj) /*! \brief This function generates a sync signal for the object. All suspended threads waiting on this sync object are resumed \param pSyncObj - pointer to the sync object control block \return upon successful signalling the function should return 0 Otherwise, a negative value indicating the error code shall be returned \note the function could be called from ISR context \warning */ #define sl_SyncObjSignal(pSyncObj) osi_SyncObjSignal(pSyncObj) /*! \brief This function generates a sync signal for the object from Interrupt This is for RTOS that should signal from IRQ using a dedicated API \param pSyncObj - pointer to the sync object control block \return upon successful signalling the function should return 0 Otherwise, a negative value indicating the error code shall be returned \note the function could be called from ISR context \warning */ #define sl_SyncObjSignalFromIRQ(pSyncObj) osi_SyncObjSignalFromISR(pSyncObj) /*! \brief This function waits for a sync signal of the specific sync object \param pSyncObj - pointer to the sync object control block \param Timeout - numeric value specifies the maximum number of mSec to stay suspended while waiting for the sync signal Currently, the simple link driver uses only two values: - OSI_WAIT_FOREVER - OSI_NO_WAIT \return upon successful reception of the signal within the timeout window return 0 Otherwise, a negative value indicating the error code shall be returned \note belongs to \ref porting_sec \warning */ #define sl_SyncObjWait(pSyncObj,Timeout) osi_SyncObjWait(pSyncObj,Timeout) /*! \brief type definition for a locking object container Locking object are used to protect a resource from mutual accesses of two or more threads. The locking object should support reentrant locks by a signal thread. This object is generally implemented by mutex semaphore \note On each porting or platform the type could be whatever is needed - integer, structure etc. \note belongs to \ref porting_sec */ #define _SlLockObj_t OsiLockObj_t /*! \brief This function creates a locking object. The locking object is used for protecting a shared resources between different threads. \param pLockObj - pointer to the locking object control block \return upon successful creation the function should return 0 Otherwise, a negative value indicating the error code shall be returned \note belongs to \ref porting_sec \warning */ #define sl_LockObjCreate(pLockObj,pName) osi_LockObjCreate(pLockObj) /*! \brief This function deletes a locking object. \param pLockObj - pointer to the locking object control block \return upon successful deletion the function should return 0 Otherwise, a negative value indicating the error code shall be returned \note belongs to \ref porting_sec \warning */ #define sl_LockObjDelete(pLockObj) osi_LockObjDelete(pLockObj) /*! \brief This function locks a locking object. All other threads that call this function before this thread calls the osi_LockObjUnlock would be suspended \param pLockObj - pointer to the locking object control block \param Timeout - numeric value specifies the maximum number of mSec to stay suspended while waiting for the locking object Currently, the simple link driver uses only two values: - OSI_WAIT_FOREVER - OSI_NO_WAIT \return upon successful reception of the locking object the function should return 0 Otherwise, a negative value indicating the error code shall be returned \note belongs to \ref porting_sec \warning */ #define sl_LockObjLock(pLockObj,Timeout) osi_LockObjLock(pLockObj,Timeout) /*! \brief This function unlock a locking object. \param pLockObj - pointer to the locking object control block \return upon successful unlocking the function should return 0 Otherwise, a negative value indicating the error code shall be returned \note belongs to \ref porting_sec \warning */ #define sl_LockObjUnlock(pLockObj) osi_LockObjUnlock(pLockObj) #endif /*! \brief This function call the pEntry callback from a different context \param pEntry - pointer to the entry callback function \param pValue - pointer to any type of memory structure that would be passed to pEntry callback from the execution thread. \param flags - execution flags - reserved for future usage \return upon successful registration of the spawn the function should return 0 (the function is not blocked till the end of the execution of the function and could be returned before the execution is actually completed) Otherwise, a negative value indicating the error code shall be returned \note belongs to \ref porting_sec \warning */ #define SL_PLATFORM_EXTERNAL_SPAWN #ifdef SL_PLATFORM_EXTERNAL_SPAWN #define sl_Spawn(pEntry,pValue,flags) osi_Spawn(pEntry,pValue,flags) //#define sl_Spawn(pEntry,pValue,flags) sl_SyncObjSignalFromIRQ(&g_pCB->ObjPool[0].SyncObj) #endif /*! Close the Doxygen group. @} */ /*! ****************************************************************************** \defgroup porting_events Event Handlers This section includes the asynchronous event handlers routines PORTING ACTION: -Uncomment the required handler and define your routine as the value of this handler @{ ****************************************************************************** */ /*! \brief \sa \note belongs to \ref porting_sec \warning */ #define sl_GeneralEvtHdlr WifiMgrGeneralEventHandler /*! \brief An event handler for WLAN connection or disconnection indication This event handles async WLAN events. Possible events are: SL_WLAN_CONNECT_EVENT - indicates WLAN is connected SL_WLAN_DISCONNECT_EVENT - indicates WLAN is disconnected \sa \note belongs to \ref porting_sec \warning */ #define sl_WlanEvtHdlr WifiMgrWlanEventHandler /*! \brief An event handler for IP address asynchronous event. Usually accepted after new WLAN connection. This event handles networking events. Possible events are: SL_NETAPP_IPV4_ACQUIRED - IP address was acquired (DHCP or Static) \sa \note belongs to \ref porting_sec \warning */ #define sl_NetAppEvtHdlr WifiMgrNetAppEventHandler /*! \brief A callback for HTTP server events. Possible events are: SL_NETAPP_HTTPGETTOKENVALUE - NWP requests to get the value of a specific token SL_NETAPP_HTTPPOSTTOKENVALUE - NWP post to the host a new value for a specific token \param pServerEvent - Contains the relevant event information (SL_NETAPP_HTTPGETTOKENVALUE or SL_NETAPP_HTTPPOSTTOKENVALUE) \param pServerResponse - Should be filled by the user with the relevant response information (i.e SL_NETAPP_HTTPSETTOKENVALUE as a response to SL_NETAPP_HTTPGETTOKENVALUE event) \sa \note belongs to \ref porting_sec \warning */ #define sl_HttpServerCallback WifiMgrHttpServerCallback /*! \brief \sa \note belongs to \ref porting_sec \warning */ #define sl_SockEvtHdlr WifiMgrSockEventHandler /*! Close the Doxygen group. @} */ #ifdef __cplusplus } #endif /* __cplusplus */ #endif /* __USER_H__ */