Hi team,
I am using the WL1801 for WIFI support. I am using the driver for Linux kernel version 3.14 and the driver is compiled and runs correctly.
During SDIO transfers between our driver and the chip, the chip seems to stop responding after awhile but always on the same SDIO request. I believe that the configuration file that is being sent to the chip during initialization is not correct.
Can you provide the chip firmware and the configuration tool which allows me to generate the chip configuration file to match the firmware for this Linux kernel version 3.14?
Currently I can't use the script found on the wiki for generating the config file because my kernel will not allow the script to complete.
Thanks for the help!
-Nick S.