This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HDMI wireless solution



Hola,

Does TI have a suitable which can meet below requirement for VR application?Thanks ~

1. HDMI input. ( if low latency and it could be uncompressed or compressed )

2. Bandwidth:

For FHD 1920*1080@60HZ w/ 3.5Gbps

For 2160*1080@90Hz w/ 8Gbps

For 4K2K 3840*2160@90Hz w/ 18Gpbs

3. Transmit distance:30m or more far