Hi,
In CC3200 lp external flash is present? if not, any external board is available only for external flash which i can link with launchpad?
Awaiting for the response on the same.
BR,
Shashank
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
In CC3200 lp external flash is present? if not, any external board is available only for external flash which i can link with launchpad?
Awaiting for the response on the same.
BR,
Shashank
Hi Shashank,
No. Example is available only for SD card. But it is relatively easy to create code to access to external flash according documentation in datasheet. As inspiration you can use driver(s) for Arduino like systems.
Jan