This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3200: Wifi AP not activated.

Part Number: CC3200
Other Parts Discussed in Thread: , UNIFLASH

Hi,

Currently working on a project which uses CC3200 as a Wi-FI Access Point. I have a binary which I am able to flash on to the CC3200 launchpad, a custom board designed with the CC3200MOD and a custom board designed with the discrete CC3200 chip. Now after flashing I am able to see the Wi-Fi access point with the launchpad and the CC3200MOD but NOT with the custom board designed with the discrete CC3200. Is there a reason for why this may be happening? The only difference is that the discrete CC3200 board is powered by a pre-regulated 1.85V. Thanks.