Other Parts Discussed in Thread: CC3220SF, CC3200
Hi,
I am using CC3220SF with simplelink SDK_1_40. In my application the simplelink enabled device has to work in station mode and have to be connected with on of the two fixed CC3220SF based AP SSIDs named Primary-XXX and Secondary-XXX.
I have to keep perform network scan in connected mode when I am connected via Secondary-XXX SSID and when Primary SSID is available then I need to switch the connection via Primary.
Here the issue is when I start scanning, I get lots of other SSID in the list but my required SSID is not due to strong signal or other parameters . Do you have any API which can just check the status of given SSID or listed SSID only.
Regards