Other Parts Discussed in Thread: UNIFLASH, CC3120
As the thread title describes, I am getting an error when I run one of the simplelink sdk wifi plugin examples (network terminal). I am using SimpleLink MSP432 SDK version 1.60.0.12 and the SimpleLink SDK WiFI plugin version 1.55.0.42. I also flashed the booster pack using uniflash and the image in the WiFi plugin.
The project builds just fine (I was having a problems building the project resolved in this thread) but when I run the program I get the following error over the UART
[ERROR] - FATAL ERROR: Sync loss detected n
[line:911, error code:-2005] Device error, please refer "DEVICE ERRORS CODES" section in errors.h
Network Terminal - Couldn't configure Network Processor
The errors.h file doesn't give any more information than what the UART prints out.
Is there anyway to tell where this issue is coming from or does anyone have any experience with this particular error?
Here are the pictures of the launchpad, boosterpack, and emulator board.