Other Parts Discussed in Thread: CC3120BOOST, CC3120, UNIFLASH, CC3100
I'm trying to connect my laptop to the board stack via WiFi. I do not see the default mysimplelink in my list of available wireless connections available. Do I need to do any config via USB/serial connection? My current goal is to be able to connect with no setup or minimal configuration.
I would like to be able to connect to CC3120BOOST out of the box without having to program a service pack. Programming the service pack is turning out to be a pain. Can't connect to device. "Error connecting to the device. Please check your COM port settings. Error code: 1" . I'm using virtual COMports COM5 thru COM8). Which comport is used and what should the settings be?