Tool/software: Linux
Hi,
I'm having weird problems with WL1805MOD as access point, where the transmission just stops suddenly until the interface is driven down and brought back up again. It can still receive packets, but transmission just hangs. Looking at /sys/kernel/debug/ieee80211/phy0/wlcore/driver_state shows that TX counters stay the same, while running iw dev wlan0 station dump shows counters increasing. This seems to happen somewhat randomly, and have not so far found a way to reliably reproduce this problem.
I've tested with couple of firmware versions and tried using latest wl18xx from upstream, but this had no effect on the issue.
These are the firmware versions I've tested:
wlcore: PHY firmware version: Rev 8.2.0.0.240
wlcore: firmware booted (Rev 8.9.0.0.75)
wlcore: PHY firmware version: Rev 8.2.0.0.242
wlcore: firmware booted (Rev 8.9.0.0.79)