Hello,
I'm currently looking for a WiFi-Sensor-Network on a bigger scale.
I've already read the user's guide of the Wi-fi SensorTag, but I still have some unanswered questions:
- How many SensorTags can approximately be connected simultaneously to the same Wifi-Network? (10, 50, 100 ?) Same question for the LaunchpadKit.
- Can I code the sensor, so it turns itself on to collect data every certain amount of time (every hour for example) and then gets back into hibernate mode?
- Is it possible to collect or access the data of a tag with different devices (tablets or smartphones) at the same time?
- Does the sensor automatically upload the data into the cloud or do I need to connect to the sensor and do it by myself each time?
- When the sensor is in hibernate mode, does it recognize a change of the surroundings and starts to collect data by itself? Or do I have to activate each sensor as soon as I need data?
- Is it possible to create a database with all the sensors and its data which I can access to from the PC?
- Is an accurate determination of the position of the sensor possible?
I know the CC3200STK-WIFIMK is intended for demonstration purposes only, so for most of these tasks I'll certainly need the LaunchpadKit. Nevertheless it would be nice if you could tell me or give me an estimation for each question, which one of the two (SensorTag or LaunchpadKit) can satisfy it or if it's even possible.
Thank you!
Kind regards,
Felix Schirrecker