Other Parts Discussed in Thread: TPA2012D2, TLV320AIC3254, , TPA2012D2EVM
Hi,
I was trying the wifi audio example and was able to transmit my audio data from one board to other. But the problem is when I tried with the 1kHz clean sine wave as input ,I can hear the sound very clear without any noise but when I checked on oscilloscope it shows that there is some kind of noise present which is may be imperceptible to human ear. I tried using external power supply but still the result is same. I read about common noise issues in audio codec and according it I should put low pass filter (1kohm resistor and 4,7nF cap) after codec but its not possible as I cannot track the path on the board . Can I put the low pass filter after the class D power amplifier at the output of speaker? Will it help?
Regards,
Charu