This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3220SF-LAUNCHXL: Retention registers

Part Number: CC3220SF-LAUNCHXL


Hi,

I am using tcpecho example and writing something to INDEX0 of the retention registers, upon wakeup the registers seems to be modified all the time.

I see from the driverlib prcm.c BIT01 to BIT14 can be used by user application even if RTC is in use.

Can someone please explain why the values are getting modified and what can I do about it?

prcm.c

//! When RTC APIs in use:
//! |-----------------------------------------------|
//! | INDEX 0 |
//! |-----------------------------------------------|
//! |31|30|29|28|27|26|25|24|23|22|21|20|19|18|17|16|
//! |-----------------------------------------------|
//! | Reserved by RTC APIs - YY |
//! |-----------------------------------------------|
//! |15|14|13|12|11|10|09|08|07|06|05|04|03|02|01|00|
//! |-----------------------------------------------|
//! |YY| For User Application |XX|
//! |-----------------------------------------------|
//!
//! YY => Reserved by RTC APIs. If Driverlib RTC APIs are used
//! XX => Reserved by ROM