The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDC-EVSE-WIFI: MSP430F6736, CC3100BOOST

Part Number: TIDC-EVSE-WIFI
Other Parts Discussed in Thread: CC3100, , CC3100BOOST

Hi, 

I have modified TIDC-EVSE-WIFI TI design as shown in attached pic. Because I didnt find CC3100_EM_BP_ADAPTUR, I mapped the pins as was described in Table 4 of TIDUBV2. I programmed both EVM and CC3100BOOST cards, but I can not see its WLAN network. I checked the definition of NHIB Mapping in board.h file of the procet, It seems it was wrong, that mapping was allocated to PILOT in design. Also the IRQ mapping is done to port P1.2. Both of them are connected to JP5 and JP6.  When I connect the CC3100BOOST to the EVM the wifi is not working. Can you please tell me how I can solve this problem?