Other Parts Discussed in Thread: CC3200, CC3235SF
First.. I am 100% new to developing electronics of any kind.
I am a programmer for web applications and I can do electronic troubleshooting and repair, however; I have never developed or created anything like what Im trying to accomplish.
I am trying to get started to build a program and load it to the CC3200STK-WIFIMK so that if it's sensors are trigger with certain parameters it pings the cloud. Which then sends an alert to my custom made app.
Where do I get started? I have tried working with the cloud composer but Im not sure if that will work because I didn't see my device when I was setting up the project. I have looked through Youtube, TI training and support and forums to find a getting started for this device specifically. Perhaps Im missing something.
I have also bought the LAUNCHPAD-CC3235SF and have seen the getting started process for that. Im hesitant to use it because I need all the sensors on the sensortag to accomplish my project and the luanchpad is missing some of them.
All your help is appreciated.
*Also open to having an experienced develop as a partner if there are that are interested on working together.