This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WL1805MOD: Interface with i.MX6 SDIO level shifter required

Part Number: WL1805MOD

I am using WL1805mod that operated on 1.8V supply, while it will interface with SDIO lines of i.MX6 which operated on 3.3V.

In this case I will require to add level shifter in the design.Any suggestions which level shifter can be used