Part Number: IMETER-BOOST
Hi ,
I used this EVM a lot and think its function is great. I used to use this tool to measure the power consumption of Zigbee and the result looks like very close to a real instrument. but recently, I re-read the user guide and datasheet of INA226, it declares that the LSB of INA226 is 2.5uV, Vos is +-2.5V, 10uV max. and a 0.1Ω shunt resistor is used. According to my understand, it should not support a current measure less than 100uA, otherwise,the offset error is too big. Please kindly comments if this boostpack is suitable for a 1uA to 10mA current measurement,? thanks.