Other Parts Discussed in Thread: UNIFLASH, CC3120, , CC31XXEMUBOOST
Hi!
I've been confused on how to include the certificates (root CA, private key, and the client certificate) to the CC3120 board using the UniFlash software in order to connect the CC3120 to Google Firebase. I found the root CA (Google Trust Services - GlobalSign Root CA-R2 certificate, which I found from this link (pki.goog )) and generated the private key to my Firebase. But the problem is that I don't know what to do after that step. I haven't come across guides out there regarding CC3120 and the addition of more certificates (on top of the default ones) to the board, if any. I've looked online for any help connecting the board to Firebase, but reading forums, such as Myo Min Min Paing's request for help on "CCS/CC3120BOOST: Issue with communication between firebase real time database and CC3120 Boost simplelink and missing root CA" (http://e2e.ti.com/support/wireless-connectivity/wifi/f/968/p/842086/3148257 ), made me even more confused.
I'm on a tight budget, so I can't really switch to another board at this point in the project.
Is there any recommendations on what I should do from here? If so, can you please give me a step-by-step list on what I should do in UniFlash?
UniFlash version: 5.1.0
Boards used: CC3120BOOST, CC31XXEMUBOOST
Any help would be greatly appreciated!
Thanks!
Justin